Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
User18058
Level 1
Level 1
Hello Sir/Madam,

We had ordered the KIT_AURIX_TC265_TFT (OPN: KITAURIXTC265TFTTOBO1) from the Infineon and now, we are unable to flash the hex file in this evaluation kit(APPLICATION KIT TC2X5 V2.0).

Its very urgent for our delivery team to test the software with this kit.

Kindly help us ASAP.

Please find the attached pics for your reference.

Grusse,
Raj
0 Likes
3 Replies
MoD
Employee
Employee
10 likes given 50 likes received 500 replies posted
Hello,
please check the labeling of the device. If it is a TC265DE then the JTAG communication is not possible. Only DAP communication possible on this device. Change the setting in your debugger to use DAP instead of JTAG for communication. If you don't know how you can do this, you must contact your debugger vendor to get the answer.
0 Likes
User18058
Level 1
Level 1
Hello,

how to connect it to DAP as there is no DAP connector on the board?
We expect from Infineon as they would have given DAP connector on the board then?

We had checked before ordering from your website and ordered as it is supported by DAP and JTAG supported:
https://www.infineon.com/cms/en/product/evaluation-boards/kit_aurix_tc265_tft/
In the above link, it says DAP and JTAG are supported but no DAP port?

Please recheck and help us.





Please refer the attached3769.attach pic for your reference.

Regards
Raj
0 Likes
MoD
Employee
Employee
10 likes given 50 likes received 500 replies posted
Winidea support DAS, you can use the USB miniWiggler on the board for debugging with winidea. For more information contact isystem. Otherwise maybe isystem has an adapter available where you can use DAP via OCDS connector.
JTAG is only available on TC265D and not on TC265DE.
0 Likes