Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Curious
Level 2
Level 2
25 sign-ins First like received 5 replies posted

Hi Community,

 

i've seen after configuration of my EVADCs that only the last defined Interrupt for the according Group is working.

At the moment the Interrupts are handled through an core. Later i want the DMA to handle the interrupt.

Is the defined Interrupt for one Channel or one Group?

And is there a difference between using the DMA instead of the Core?

My Code is similiar to the one of srgbtl:

Interrupt generation with multiple ADC channel - Infineon Developer Community

Thanks in advance

Andreas

 

0 Likes
1 Solution
FD_aurix
Level 5
Level 5
100 sign-ins 100 replies posted 5 solutions authored

you need to put your code, it will be easier.

In any case the channels that activate the interrupt at the EOC are selected by ENSI bit when you define the queue. If you have more than one on the same QUEUE they activate the same interrupt

View solution in original post

0 Likes
1 Reply
FD_aurix
Level 5
Level 5
100 sign-ins 100 replies posted 5 solutions authored

you need to put your code, it will be easier.

In any case the channels that activate the interrupt at the EOC are selected by ENSI bit when you define the queue. If you have more than one on the same QUEUE they activate the same interrupt

0 Likes