- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Ifx community,
I am reading the Tc3XX user manual. Since the SDA pin is an I/O pin, used for output, it should be configured as Alt(5).
I wonder if, for a write operation, it needs to be configured as O(5) first, and for a read operation, it needs to be configured as an input first.
in AURIX_TC3xx_Part1-UserManual-v02_00-EN.pdf
14.2
If a peripheral unit uses a GPIO port line as a bi-directional I/O line, register Pn_IOCR has to be written for input or output selection. The Pn_IOCR register further controls the driver type of the output driver, and determines whether an internal weak pull-up, pull-down, or without input pull device is alternatively connected to the pin when used as an input. This offers additional advantages in an application
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Digital inputs are enabled by default (if there is an analog input on that pin they can be disabled). With I2C you should used the open drain selection for O(5).
In your code you need to write the IOCRx register with your setting for the pin.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Digital inputs are enabled by default (if there is an analog input on that pin they can be disabled). With I2C you should used the open drain selection for O(5).
In your code you need to write the IOCRx register with your setting for the pin.