How to understand the register MCi_RANGE in TC377

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
ASUS
Level 2
Level 2
10 replies posted 5 questions asked 5 replies posted

Hi,

I'm confused about the register MCi_RANGE. For example, the register MC10_RANGE (for CPU2_DMEM) has a default value of 0xB780, correspondingly, RAEN=0, UPLIMIT=0x6F, LOLIMIT=0x00. 

But in memmap we can see the size of CPU2_DMEM is 0x1C000, please tell me the method of translate 0x6F to 0x1C000 or 0x1BFFF.

And if I want to inject an ECC error at address 0x50010000, how to config this register?

What's the means of "limit in 64 word increments" and "UPLIMIT & 111111B"?

MCi_RANGE.png

Best regards

ASUS

0 Likes
1 Solution
µC_Wrangler
Employee
Employee
50 solutions authored 100 sign-ins 25 likes received

Hi ASUS.  To get to the underlying math, you need to look in the TC37x variant-specific appendix (TC37x_appx_um_v2.0.pdf).  The table in question is Table 57 SSH instances, which shows this for CPU0_PMEM: Mux factor 8

98304 bytes / (64-bit width for PSPR/PCACHE) / (2 ^ Mux factor 8 ) = 48, which corresponds to RANGE=0x2F

If you want to inject an error at a single address, see 13.3.5.1.7 Writing to a Single Memory Location  in the User Manual.

View solution in original post

0 Likes
5 Replies
ASUS
Level 2
Level 2
10 replies posted 5 questions asked 5 replies posted

Hello? I want to know that, pls

0 Likes
ub786
Level 3
Level 3
10 replies posted First solution authored 10 sign-ins

Hi,


0x70 * 0x400 = 0x1C000 (112x1024 = 114688)

as
lower limit = 0x0
Upper Limit = 0x6F

Which leads to total of 0x70 KB (112*1024) of size.

BR

0 Likes
ASUS
Level 2
Level 2
10 replies posted 5 questions asked 5 replies posted

Hi,

Thank you for your reply. Could you tell me what is 0x400? It's said 64 word in usermanual, so 1 word is 16 byte?

 

For another memory, CPU0_PMEM, the default value of UPLIMIT is 0x2F, and the size is 96kbyte, 0x00018000, how to get 0x2F from 0x00018000?

ASUS_0-1657680012863.png

ASUS_1-1657680033149.png

 

Best Regards

ASUS

0 Likes
Nambi
Moderator
Moderator
Moderator
500 replies posted 50 likes received 5 likes given

Hi,

We reiterate the recommendation from the user manual.

The recommendation is always to do full range tests (i.e. RANGE.RAEN = 1 and RANGE.ADDR = full range). When trying to test a single memory location using the MBIST, the user should read and write using the same settings for the RANGE register.

Best Regards.

0 Likes
µC_Wrangler
Employee
Employee
50 solutions authored 100 sign-ins 25 likes received

Hi ASUS.  To get to the underlying math, you need to look in the TC37x variant-specific appendix (TC37x_appx_um_v2.0.pdf).  The table in question is Table 57 SSH instances, which shows this for CPU0_PMEM: Mux factor 8

98304 bytes / (64-bit width for PSPR/PCACHE) / (2 ^ Mux factor 8 ) = 48, which corresponds to RANGE=0x2F

If you want to inject an error at a single address, see 13.3.5.1.7 Writing to a Single Memory Location  in the User Manual.

0 Likes