Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Ptar
Level 1
Level 1
5 likes given 10 sign-ins 5 replies posted

As per 13.3.5.1.6 Reading a Single Memory Location, if I configure the register, I can access single address to read.
But If I give, RAEN= 0, MCi_RANGE.ADDR (Where i = 1 CPU0 DTAG) = 0000000000000b which is of 14bits. Which memory location of DTAG will be accessed? How does 14bits mapped to 32bits address.

0 Likes
1 Solution
Jeremy_Z
Moderator
Moderator
Moderator
1000 replies posted 250 sign-ins 100 likes received

Hi @Ptar ,

Cache Ram and cache Tag Ram are used automatically when the cache is switched on. There is nothing to define in the linker script file for this memory. So please note that Cache Ram and Cache Tag Ram are not directly accessible by any CPU or debugger, so I consider it's the root cause that you fail to watch the variable in the RAM area.

BR,

Jeremy

View solution in original post

0 Likes
6 Replies
Ptar
Level 1
Level 1
5 likes given 10 sign-ins 5 replies posted

The offset address will be from 0000h to 17ffh, that means 14bits are enough to represent the offset address. right? 0001 0111 1111 1111 -> 1 0111 1111 1111.

As per my understanding, what ever address we give in MCi.ADDR is offset address of CPU0 DTAG RAM when i = 1

0 Likes
Jeremy_Z
Moderator
Moderator
Moderator
1000 replies posted 250 sign-ins 100 likes received

Hi @Ptar ,

1) The offset address will be from 0000h to 17ffh, that means 14bits are enough to represent the offset address. right?

-- Yes, it's right.

Further, I'd like to suggest you refer to the MTU_MBIST demo to implement read values from the DTAG RAM.

BR,

Jeremy

 

Ptar
Level 1
Level 1
5 likes given 10 sign-ins 5 replies posted

Hi @Jeremy_Z ,


OK. I will check. If we write data to DTAG using single address mode (MC.RANGE = 0X00), the data at mentioned address only will be modified, right?  

I have tried to read the data from DTAG RAM address 700C 0000 and used view-->dump option to view CPU0 DTAG RAM memory.

The data present in the address was 700C 0000: 0000 0000  ???? ????

But when read the 700C 0000 using the RDBFL register, the value is as following.

RDBFL0: 0001
RDBFL1: 0088
RDBFL2:0000
RDBFL3:0011

But these values are not seen while viewing via view->dump -> 700C 0000.

Whether DTAG RAM address is viewable in View-->dump?

0 Likes
Jeremy_Z
Moderator
Moderator
Moderator
1000 replies posted 250 sign-ins 100 likes received

Hi @Ptar ,

Actually, I was wondering if you can illustrates the steps of the above testing, so then I can replicate the phenomenon and it can help me to figure it out.

BR,

Jeremy

0 Likes
Ptar
Level 1
Level 1
5 likes given 10 sign-ins 5 replies posted

Hi @Jeremy_Z 

  1. View -> Dump -> CPU0 DTAG Address (700C 0000H)
  2. Disable the SMU Alarm
  3. Enable the DTAG SSH
  4. Perform DTAG SRAM Read from 700C 0000H (offset address 0x0000) (13.3.5.1.6 Reading a Single Memory Location)
  5. Store value in RDBFL to a variable
  6. Disable SSH
  7. Enable SMU Alarm
  8. View -> dump -> 700c 0000H.
  9. The value in the variable and at the address 700C 0000H shall be same
0 Likes
Jeremy_Z
Moderator
Moderator
Moderator
1000 replies posted 250 sign-ins 100 likes received

Hi @Ptar ,

Cache Ram and cache Tag Ram are used automatically when the cache is switched on. There is nothing to define in the linker script file for this memory. So please note that Cache Ram and Cache Tag Ram are not directly accessible by any CPU or debugger, so I consider it's the root cause that you fail to watch the variable in the RAM area.

BR,

Jeremy

0 Likes