Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

JexJiang
Level 2
Level 2
First solution authored 10 replies posted 10 sign-ins

Hi:

How to erase and read Pflash0 on CPU2 on TC39x MCU, when CPU0 has code to execute (CPU0 will access Pflash0, resulting in Contexmangagementrap)? After testing, it is possible for CPU2 to erase and read Pflash2. The API of erasing and reading has been memcpy into PSPR

0 Likes
1 Solution
µC_Wrangler
Employee
Employee
100 sign-ins 25 likes received 25 solutions authored

The TC3xx doesn't support writing to PFLASH while any bus master is reading from that same physical bank.  That applies to all bus masters: not just CPUs, but also the HSM (if enabled), DMA, and Ethernet.

So, you'll need to ensure that other CPUs are either idle, or executing from RAM.  Make sure you either disable periodic interrupts (STM, GTM, etc.) that might still be occurring, or move both the BIV of other CPUs and the interrupt handlers into RAM.

View solution in original post

0 Likes
2 Replies
µC_Wrangler
Employee
Employee
100 sign-ins 25 likes received 25 solutions authored

The TC3xx doesn't support writing to PFLASH while any bus master is reading from that same physical bank.  That applies to all bus masters: not just CPUs, but also the HSM (if enabled), DMA, and Ethernet.

So, you'll need to ensure that other CPUs are either idle, or executing from RAM.  Make sure you either disable periodic interrupts (STM, GTM, etc.) that might still be occurring, or move both the BIV of other CPUs and the interrupt handlers into RAM.

0 Likes

Dear µC_Wrangler:

      Thanks for your reply.

0 Likes