Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
User19978
Level 1
Level 1
Hi...

I am working on TC297....

Example code has been given for to change the intensity of single LED...
Please Help to do the same for 6 LEDs

void initGtmTomPwm(void)
{
IfxGtm_enable(&MODULE_GTM); /* Enable GTM */

IfxGtm_Cmu_enableClocks(&MODULE_GTM, IFXGTM_CMU_CLKEN_FXCLK); /* Enable the FXU clock */

/* Initialize the configuration structure with default parameters */
IfxGtm_Tom_Pwm_initConfig(&g_tomConfig, &MODULE_GTM);

g_tomConfig.tom = LED.tom; /* Select the TOM depending on the LED */
g_tomConfig.tomChannel = LED.channel; /* Select the channel depending on the LED */
g_tomConfig.period = PWM_PERIOD; /* Set the timer period */
g_tomConfig.pin.outputPin = &LED; /* Set the LED port pin as output */
g_tomConfig.synchronousUpdateEnabled = TRUE; /* Enable synchronous update */

IfxGtm_Tom_Pwm_init(&g_tomDriver, &g_tomConfig); /* Initialize the GTM TOM */
IfxGtm_Tom_Pwm_start(&g_tomDriver, TRUE); /* Start the PWM */
}
0 Likes
0 Replies