Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

User19909
Level 3
Level 3
First like received
Hello,

I am having trouble calculating EVADC conversion time, how can I know the frequency used by adc, in the clocking system chapter it is mentioned that fadc = fsource1, is fsource1 same as fpll1? if so I have fpll1 =300Mhz, so is fadc now 300MHZ and fadci = fadc/(DIVA+1)?

it seems something in my understanding is incorrect so please correct me.
0 Likes
4 Replies
cwunder
Employee
Employee
50 solutions authored 250 sign-ins 25 likes received
I would expect that you would configure PLL1 to be set to 320MHz and then bit CCUCON1.PLL1DIVDIS=0 so you would get a divide by 2 for fSOURCE1 (160MHz). The maximum input clock frequency for the EVADC is 160MHz
0 Likes
User19909
Level 3
Level 3
First like received
and what is NCR in the conversion time formula, how can I get this configured value?
0 Likes
cwunder
Employee
Employee
50 solutions authored 250 sign-ins 25 likes received
TC37xx wrote:
and what is NCR in the conversion time formula, how can I get this configured value?

I am not sure where NCR is coming from. Looking at the users manual under section 32.9.2 Standard Convert Channels Timing:
tC12 = [(2 + STC) × tADCI] + [13 × tADCI] + [NRS × tNR] + [tPC] + [3 × tADC]
with:
tNR = 4 × tADCI + 3 × tADC per conversion step
tPC = (4 + 2×CALSTC) × tADCI + 5 × tADC if enabled, otherwise 0
0 Likes
User19909
Level 3
Level 3
First like received
I am having some trouble with calculating the conversion time, I have now derived all the required parameters to substitute in the conversion time formula, however the result I am getting is far from what I observe if I calculate the conversion time with STM.

Fosc is configured to be 20Mhz. NDIV+1 and PDIV+1 in PERPLLCON as 28 and 1, KDIV2+1 is 5. so I derived from the following Fpll1 = 112Mhz, and from CCUCON1.PLL1DIVDIS=1 and CLKSEL =01, Fsource1=fpl11, so Fsource1= Fadc =112 MHz, is there something wrong here ?

Step 2
STC=256
FadcI=Fadc/DIVA = 112/32 = 3.5 MHz
NRS=7
CALSTC=3
so from the following and the equation @cwunder mentioned I calculated the conversion time to be 88544 usec, is there something I need to multiply or add to Tc12 or is this the total conversion time? What I am getting from the STM is around 99192 usec consistently.
0 Likes
This widget could not be displayed.