Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

User17740
Level 3
Level 3
First like received
Hi,

How many of the CAN nodes are capable of CAN FD in AURIX?

#8042000 12023
0 Likes
2 Replies
User17270
Level 1
Level 1
First like received
For the TC397 silicon that I have used all 12 nodes are FD capable.
0 Likes
User17612
Level 3
Level 3
First like received
Hi,

In the errata sheets the point*MultiCAN_TC.H008 shows information that need to be checked regarding*ISO 11898-1:2015 compatibility.
ISO compatible CAN FD variants have a N at the end like in*SAK-TC234LP-32F200*N*. The information is applied in the Errata Sheet to consider latest changes of the ISO11898
Also a table is provided there showing exactly the nodes with ISO CAN FD supporting nodes (example form TC23x AC):

3714.attach
0 Likes