Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

Not applicable
In Infineon Aurix TX29x B-Step
32-bit Single-Chip Microcontroller
User's Manual V1.3 2014-12, are General Purpose I/O Ports Base Address(GPIO) in contradiction?

In Chapter 13.3.2, P0n_IOCR0 (n = 0 - 2) matches the base address of (0xF003A010 + n * 0x100) specified in Table 13-3 and Table 13-4.
In Chapter 13.3.2, for Pn_IOCR0 (n = 10-11), base address is (0xF003A610 + n * 0x100) but for these same registers, address in Table 13-3 is specified at 0xF003B000?

Other GPIO Base Addresses in Chapter 13.3.2 are in contradiction as well?

I'm new to Tricore. Is this a mistake in User's Manual?
0 Likes
2 Replies
cwunder
Employee
Employee
50 solutions authored 250 sign-ins 25 likes received
I don't recognized the issue can you more clearly state the contradiction?

Table 13-3 Register Address Space states the Base Address for P10 it is 0xF003B000 that is also P10_OUT. To calculate Pn_IOCR0 (n=10) its address is 0xF003A610 + n * 0x100. So 0xF003A610 + 0xA00 = 0xF003B010, The Pn_IOCR0 is the base address plus offset of 0x10 as listed in Table 13-4 Registers Overview.
0 Likes
Not applicable
There is no contradiction. I was calculating Pn_IOCR0 address incorrectly. Thank you for correcting me.
0 Likes