Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

User16898
Level 4
Level 4
Hi,

I'm trying to configure GMT timer.

The problem is that, result frequency is different than the one i set.
I have following init function:

void gtm_timers_initialization(void){

boolean interruptState = IfxCpu_disableInterrupts();

/* set Gtm clock frequency */
float32 gtm_frequency = IfxGtm_Cmu_getModuleFrequency(gtm);
IfxGtm_enable(gtm);

IfxGtm_Cmu_setGclkFrequency(gtm, gtm_frequency);

IfxGtm_Tom_Timer_Config timerConfig;

IfxGtm_Tom_Timer_initConfig(&timerConfig, gtm);

/* power switch timer */
timerConfig.base.frequency = 100; //100Hz
timerConfig.base.minResolution = (1.0/timerConfig.base.frequency)
/TIMER_RESOLUTION_DIVIDER;
timerConfig.base.isrProvider = ISR_PROVIDER(INTERRUPT_TIMER_10MS);
timerConfig.base.isrPriority = ISR_PRIORITY(INTERRUPT_TIMER_10MS);
timerConfig.base.trigger.enabled = FALSE;
timerConfig.tom = IfxGtm_Tom_0;
timerConfig.timerChannel = IfxGtm_Tom_Ch_0;
timerConfig.clock = IfxGtm_Tom_Ch_ClkSrc_cmuFxclk0;
IfxGtm_Tom_Timer_init(&tom_timer, &timerConfig);

IfxCpu_restoreInterrupts(interruptState);

IfxGtm_Cmu_enableClocks(gtm,
IFXGTM_CMU_CLKEN_FXCLK | IFXGTM_CMU_CLKEN_CLK0);
IfxGtm_Tom_Timer_run(&tom_timer);

}


I also use timer interrupts.
IFX_INTERRUPT(ISR_Timer_10ms, 0, ISR_PRIORITY_TIMER_10MS){
if(switch_timer % 2 == 0){
switch_on_pin();
}else{
switch_off_pin();
}
switch_timer++;
}


The problem is, that the frequency of setting/resenting is complettly different than the one i set.
if I set timerConfig.base.frequency = 100 (Hz) which is 10 ms period, interrupt is firing in 450 us period (2.2 kHz).
If I set timerConfig.base.frequency = 1000(Hz) which is 1ms, interrupt is firing in 45 us period (22.2 kHz).

As source I use PLL that is ramped-up to 133.33 MHz, f_source = 133.33 MHz.
f_GTM = f_ source


Why GTM timer is setting completely different frequency than those configured?
I work on Tc222L
0 Likes
1 Reply
User16898
Level 4
Level 4
Problem solved,

It turns out tha iLLD library supports only 100,200 Mhz frequencies. Setting every different result in shitty GTM timer frequency.
Moreover GTM module is doubling input frequency, if ones want to have fGtm = 100 MHz, they must provide 50 Mhz frequency ( GTMDIV = fsource/2).
0 Likes