Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

User19905
Level 1
Level 1
Hi,

I am new to Aurix and using Tricore TC275TP-64.
I want to know(I saw T3 can be reload using T2/T4 timers with relaod values in example project) whether we can use T2, T3, T4 timers independely with different reload time value in timer mode to create interrupts.
I understood, I can get interrupts when these timers overflow(65535) but can I choose the value to timeout?

I was trying as below to generate 200ms and 1000ms interrupts.
void initGpt12Timer(void)
{
/* Initialize the GPT12 module */
IfxGpt12_enableModule(&MODULE_GPT120); /* Enable the GPT12 module */
IfxGpt12_setGpt1BlockPrescaler(&MODULE_GPT120, IfxGpt12_Gpt1BlockPrescaler_16); /* Set GPT1 block prescaler */

/* Initialize the Timer T3 */
IfxGpt12_T3_setMode(&MODULE_GPT120, IfxGpt12_Mode_timer); /* Set T3 to timer mode */
IfxGpt12_T3_setTimerDirection(&MODULE_GPT120, IfxGpt12_TimerDirection_down); /* Set T3 count direction */
IfxGpt12_T3_setTimerPrescaler(&MODULE_GPT120, 2); /*prescalar-64; Set T3 input prescaler */
IfxGpt12_T3_setTimerValue(&MODULE_GPT120,19531); /* 200ms */
/* Initialize the interrupt */
volatile Ifx_SRC_SRCR *src = IfxGpt12_T3_getSrc(&MODULE_GPT120); /* Get the interrupt address */
IfxSrc_init(src, IfxSrc_Tos_cpu1, 1); /* Initialize service request */
IfxSrc_enable(src); /* Enable GPT12 interrupt */
IfxGpt12_T3_run(&MODULE_GPT120, IfxGpt12_TimerRun_start); /* Start the timer */

/* Initialize the Timer T2 */
IfxGpt12_T2_setMode(&MODULE_GPT120, IfxGpt12_Mode_timer); /* Set T2 to timer mode */
IfxGpt12_T2_setTimerDirection(&MODULE_GPT120, IfxGpt12_TimerDirection_down); /* Set T2 count direction */
IfxGpt12_T2_setTimerPrescaler(&MODULE_GPT120, 3); /* Prescalar:128 - T2 input prescaler */
IfxGpt12_T2_setTimerValue(&MODULE_GPT120, 48828); /* Set T2 start value */
/* Initialize the interrupt */
src = IfxGpt12_T2_getSrc(&MODULE_GPT120); /* Get the interrupt address */
IfxSrc_init(src, IfxSrc_Tos_cpu1, 2); /* Initialize service request */
IfxSrc_enable(src); /* Enable GPT12 interrupt */
IfxGpt12_T2_run(&MODULE_GPT120, IfxGpt12_TimerRun_start); /* Start the timer */
}

IFX_INTERRUPT(T2ISR, 0, 1)
{....
}
IFX_INTERRUPT(T3ISR, 0, 2)
{...
}

Currently my ISR are hittling on 671ms and 1342ms.

I would like to use 5 different timer values through out my program to schedule different state machines in code.
0 Likes
2 Replies
cwunder
Employee
Employee
50 solutions authored 250 sign-ins 25 likes received
I am not sure where you got your timeout values. Typically the frequency of the SPB is 100MHz and this is the clock source for the GPT12.

Here is an example to configure T2 (200ms) and T3 (1 second).

Port pins P00.0 and P00.1 show the timeouts by toggling pins in their ISR's


#define T2_RELOAD 9765
#define T3_RELOAD 48828
volatile uint32 T2_ticks;
volatile uint32 T3_ticks;

void GPT12_Init(void){
uint16 cpuWdtPassword = IfxScuWdt_getCpuWatchdogPassword();

IfxScuWdt_clearCpuEndinit(cpuWdtPassword);
GPT120_CLC.U = 0; /* enable peripheral and allow sleep mode */
(void) GPT120_CLC.U;
IfxScuWdt_setCpuEndinit(cpuWdtPassword);


P00_IOCR0.B.PC0 = PCx_Output_PushPull_gpio;
P00_IOCR0.B.PC1 = PCx_Output_PushPull_gpio;

/* Enter interrupt level and initialize both the SCR and jump table entry */
SRC_GPT120T2.U = TOS_CPU0 | SRE_ON | SRPN_CPU0_GPT120_T2;
/* Enter interrupt level and initialize both the SCR and jump table entry */
SRC_GPT120T3.U = TOS_CPU0 | SRE_ON | SRPN_CPU0_GPT120_T3;

/* setup the */
Ifx_GPT12_T3CON t3con =
{
.B.T3I = TxI_TimerInputPrescaler_64,
.B.T3M = TxM_TimerMode,
.B.T3R = TxR_TimerRun_stop,
.B.T3UD = TxUD_CountsDown,
.B.T3UDE = TxUDE_TimerDirectionSource_internal,
.B.T3OE = 0,
.B.T3OTL = 0,
.B.BPS1 = BPS1_DivBy32,
.B.T3EDGE = 0,
.B.T3CHDIR = 0,
.B.T3RDIR = TxUD_TimerDirection_down
};
GPT120_T3CON.U = t3con.U;
(void) GPT120_T3CON.U;


/* setup the */
Ifx_GPT12_T2CON t2con =
{
.B.T2I = TxI_TimerInputPrescaler_64,
.B.T2M = TxM_TimerMode,
.B.T2R = TxR_TimerRun_stop,
.B.T2UD = TxUD_CountsDown,
.B.T2UDE = TxUDE_TimerDirectionSource_internal,
.B.T2RC = 0,
.B.T2IRDIS = 0,
.B.T2EDGE = 0,
.B.T2CHDIR = 0,
.B.T2RDIR = 0
};
GPT120_T2CON.U = t2con.U;
(void) GPT120_T2CON.U;

/* T2 start value */
GPT120_T2.U = T2_RELOAD;


/* T3 start value */
GPT120_T3.U = T3_RELOAD;


/*stop timers when debugger stops */
GPT120_OCS.U = 0x11000000;

/* start timer 2 */
GPT120_T2CON.B.T2R = 1;
/* start timer 3 */
GPT120_T3CON.B.T3R = 1;
}


The ISR's

IFX_INTERRUPT(GPT12_T2ISR, VECTAB0, SRPN_CPU0_GPT120_T2);
void GPT12_T2ISR(void)
{
GPT120_T2.U = T2_RELOAD;
P00_OMR.U = PORT_TGL_P0;
T2_ticks++;
}

IFX_INTERRUPT(GPT12_T3ISR, VECTAB0, SRPN_CPU0_GPT120_T3);
void GPT12_T3ISR(void)
{
GPT120_T3.U = T3_RELOAD;
P00_OMR.U = PORT_TGL_P1;
T3_ticks++;
}


Scope plot
0 Likes
User19905
Level 1
Level 1
Thanks a lot. It is working now. I was not reloading the timer in ISR earlier.
0 Likes
This widget could not be displayed.