GETH - Dynamic per Packet Routing

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
User18757
Level 1
Level 1
5 questions asked First like received First reply posted
(Board: TriBoard TC3x7 TH V2.01)

Hi,

referencing the 3xx Manual 44.3.9.5.2, it should be possible to route a packet based on the destination address to a spedific DMA channel.

There should be DCS set with (0x1 for e.g. DMA channel 1) of the specific MAC Address register - if the DA of the packet matches, it should be routed to DMA channel 1.
Also the Q0DDMACH of the MTL_RXQ_DMA_MAP0 should be set to 0x1.

But with this config the packets remain in Q0. Anything else needed?
Is there a special Hw_Feature needed?

PS: The static mapping with Q0MDMACH to channel 1 works fine.

Thanks,
Greetings
0 Likes
0 Replies