Announcements

Help us improve the Power & Sensing Selection Guide. Share feedback

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
manojkp04
Level 1
Level 1
First reply posted First question asked Welcome!

Hello Team,

I am using TC375. I am performing voltage tests (Under voltage 4.7V for 5sec and Normal Voltage 13V for 15sec) in 30 loops. In some situation after entering 13V, the Flexray communication is not started or started with the delay (2s to 5s). But the CAN communication is started.

On further analysis we found that the Clock Correction Failed Counter is exceeding the “maximum without clock correction fatal” limit defined by SUCC3.WCF

The flexray is trying to recover multiple times, but it is not successful and it is unable to resynchronize with the bus.

Please refer to the attached snapshots and logs. 

This is an high priority issue and needs immediate resolution

0 Likes
3 Replies
Di_W
Moderator
Moderator
Moderator
500 solutions authored 1000 replies posted 250 solutions authored

 。

0 Likes
manojkp04
Level 1
Level 1
First reply posted First question asked Welcome!

@Di_W Your reply is empty. Do you want to say something?

0 Likes
xiaoxuan
Level 3
Level 3
50 sign-ins 25 replies posted 25 sign-ins

Hello,

I am developing flexray function of TC375. Could you please send me a routine of E_Ray module, or the reading materials about E_Ray module

Looking forward to your reply

0 Likes