- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
We have just started on AURIX MCU. We have developed and tested the code using ADS. However, we have our own custom boards which we wanted to flash.
We have Lauterbach debugger currently, is it possible to flash via lauterbach?
If Yes, how do we connect the ADS to lauterbach device which is a Hardware.
If No, please suggest easiest way to flash the SW.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
T32 is is not integrated wtih ADS. However I would say you can use the standard tool flow with Lauterbach. Typically you would have setup using the T32Start for the with your options.
To you program your software into the AURIX device you would run the flash cmm file for the TC37x one you have opened T32 and connected to the TC377. If you have the T32 installed in the default directories you would run C:\T32\demo\tricore\flash\tc37x.cmm
Note you can also directly flash you program into the device from ADS
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
T32 is is not integrated wtih ADS. However I would say you can use the standard tool flow with Lauterbach. Typically you would have setup using the T32Start for the with your options.
To you program your software into the AURIX device you would run the flash cmm file for the TC37x one you have opened T32 and connected to the TC377. If you have the T32 installed in the default directories you would run C:\T32\demo\tricore\flash\tc37x.cmm
Note you can also directly flash you program into the device from ADS
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Thank you for the detailed explanation.
For, flashing the program directly through ADS , some Hardware will be required right? To communicate from PC to the JTAG connector. What should be that Hardware (currently we only have lauterbach)?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Generally, ADS is using integrated debugger for onboard miniWiggler of Tribaord which simulate a COM port on the PC with Win10 system.
You can use other debugger(i.e. PLS) with .elf file generated by ADS which is using a free Tasking compiler.
But this debug process is separated with build process.