Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

This widget could not be displayed.
Not applicable
Hi,

What is a good, simple, inexpensive debug / flash program solution? There seem to be a lot of choices out there. I will be using it on a TC375 with a custom board.
Ideally, it would work within the Aurix Development Studio.

Thank you,
Charlie
0 Likes
1 Reply
This widget could not be displayed.
Not applicable
I seem to ask the wrong questions. Sorry. I like the way the debugger / flash programmer works on the dev board. I see that it has a FTDI chip which translates USB to UART and JTAG? (I think it is JTAG but it could be DAP) The FTDI data sheet explains this pretty well.
It also has an EEPROM hooked up to it. Is this necessary for use as a debugger or an extra feature of the dev board? If it is necessary, is the image available? This is a lot to grasp and I need some help.

Thanks,
Charlie
0 Likes
This widget could not be displayed.