Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

ub786
Level 3
Level 3
10 replies posted First solution authored 10 sign-ins

Hi,

Is it possible to use GREFCLK instead of REFCLKA for RMII interface (TC38xx)?

P11.5 instead of P11.12?

Thank you for your help

BR

 

0 Likes
1 Solution
dw
Moderator
Moderator
Moderator
1000 replies posted 250 solutions authored 100 likes received

Hi ub786,

dw_0-1646135985830.png

From the user manual TC3xx and TS appx, you can find EPR field 100b leads that RMII is selected and an internal predivider divides the clock clk_rmii_i from pin ETHRXC by 2 or 20 and provides it to the internal signals clk_tx_i and clk_rx_i. And clk_rmii_i is 50-MHz clock used by the RMII from PHY.

 

View solution in original post

1 Reply
dw
Moderator
Moderator
Moderator
1000 replies posted 250 solutions authored 100 likes received

Hi ub786,

dw_0-1646135985830.png

From the user manual TC3xx and TS appx, you can find EPR field 100b leads that RMII is selected and an internal predivider divides the clock clk_rmii_i from pin ETHRXC by 2 or 20 and provides it to the internal signals clk_tx_i and clk_rx_i. And clk_rmii_i is 50-MHz clock used by the RMII from PHY.