Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

User18303
Level 2
Level 2
Hi all,

Does DAVE™ support AURIX™ family?

Best regards,
Lina


#8042000 13389
0 Likes
1 Reply
User18237
Level 5
Level 5
First solution authored First like received
Hi Lina,

Infineon DAVE™ (D igital A pplication V irtual E ngineer), a well known free of charge C/C++-language software development and code generation tool for microcontroller applications, support the XMC Microcontroller family only.
However, for AURIX™ TC2x Infineon provides the AURIX™ Development Studio. It can be downloaded from http://www.infineon.com/aurixdevelopmentstudio. The AURIX™ Development Studio is a free of charge Integrated Development Environment (IDE) for the TriCore™-based AURIX™ microcontroller family. It is a comprehensive development environment, including Eclipse IDE, C-Compiler, Multi-core Debugger, Infineon low-level driver (iLLD), with no time and code-size limitations that enables editing, compiling, and debugging of application code. Combined with numerous code example projects, the IDE can be used to evaluate the powerful architecture of the AURIX™ microcontroller family. In 2020 support for AURIX™TC3xx will be added.
Additionally, the Infineon Software Framework and its successor BIFACES are the build framework can be used to achieve similar purposes with more flexibility. Such build framework provides the possibility to integrate different tools, which work together to create an executable file for required targets.

Best regards,
Mr. AURIX™
0 Likes