Different VC_IN voltage of the eval board

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Charlie9527
Level 2
Level 2
5 questions asked 10 sign-ins 5 replies posted
Hi
 
I can see there are many different eval board of AURIX with different voltage.
What is the difference of 3V3 and 5V?
 
0 Likes
1 Solution
Di_W
Moderator
Moderator
Moderator
500 solutions authored 1000 replies posted 250 solutions authored

Hi Charlie,

For Triboard, all needed voltages are generated via Infineon’s Multi Voltage Safety Micro Processor Supply TLF35584QV and via the microcontroller itself (+1,25V).
The supply device is available as two different devices:
TLF35584QVVS1 -> +5V standby voltage, +5V TriCore™ supply (V_UC)
TLF35584QVVS2 -> +3,3V standby voltage, +3,3V TriCore™ supply (V_UC)
Dependent of the assembled device the board works with 5V or 3,3V IO.
The TLF35584QV provide the following voltages:
+3,3V or +5V for standby (connected to VEVRSB)
+3,3V or +5V for TriCore™ (connected to VEXT)
+5V communcation supply (used by CAN and FlexRay™ transceivers)
+5V voltage reference (connected to VDDM and VAREFx)
+3,3V via LDO directly from pre regulator
Applying a stable supply voltage causes the power on reset after a short period. The three LED's (V_UC, +3.3V,
VDD) indicate the status of the on board generated voltages.
A manual power on reset is executed by pressing the reset button.
The Board has to be connected to a +3,5V to +40V DC power supply.
The power consumption is not specified yet but a supply with 12V and 500mA is recommended. \

Below is screenshot of the sch for your reference which is from TriboardManualxxx.pdf

dw_0-1655276278153.png

dw

View solution in original post

3 Replies
Di_W
Moderator
Moderator
Moderator
500 solutions authored 1000 replies posted 250 solutions authored

Hi Charlie,

For Triboard, all needed voltages are generated via Infineon’s Multi Voltage Safety Micro Processor Supply TLF35584QV and via the microcontroller itself (+1,25V).
The supply device is available as two different devices:
TLF35584QVVS1 -> +5V standby voltage, +5V TriCore™ supply (V_UC)
TLF35584QVVS2 -> +3,3V standby voltage, +3,3V TriCore™ supply (V_UC)
Dependent of the assembled device the board works with 5V or 3,3V IO.
The TLF35584QV provide the following voltages:
+3,3V or +5V for standby (connected to VEVRSB)
+3,3V or +5V for TriCore™ (connected to VEXT)
+5V communcation supply (used by CAN and FlexRay™ transceivers)
+5V voltage reference (connected to VDDM and VAREFx)
+3,3V via LDO directly from pre regulator
Applying a stable supply voltage causes the power on reset after a short period. The three LED's (V_UC, +3.3V,
VDD) indicate the status of the on board generated voltages.
A manual power on reset is executed by pressing the reset button.
The Board has to be connected to a +3,5V to +40V DC power supply.
The power consumption is not specified yet but a supply with 12V and 500mA is recommended. \

Below is screenshot of the sch for your reference which is from TriboardManualxxx.pdf

dw_0-1655276278153.png

dw

Di_W
Moderator
Moderator
Moderator
500 solutions authored 1000 replies posted 250 solutions authored

Otherwise, you could refer to AURIXTC3xx_ts_part1_v2.5.1.pdf HWCFG[2:1] setting explaination of Table 466 Supply Mode and Topology selection as below showed:

dw_1-1655277102437.png

 

Thanks a lot.

0 Likes