Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

This widget could not be displayed.
Not applicable
Hi,

I have KIT_AURIX_TC297.
I want to debug it using the JTAG and DAP miniWiggler.
I am using Free TriCore Entry Toolchain. But the UDE that comes with is of limited version and does not allow me to connect the board using either JTAG or DAP miniWiggler.
Is there any way I can get Standard version of UDE for free download which allows this type of debugging?

Or any other tool is available for this task??

Your quick help is appreciated.

Regards,
Divya
0 Likes
2 Replies
This widget could not be displayed.
Not applicable
Hello Divya

I do believe the free toochain works with Miniwiggler (V3) and DAP.
Please note that Infineon DAS must be installed also (http://www.infineon.com/cms/en/product/promopages/das/)

Vincent
0 Likes
User14560
Level 1
Level 1
Hi,

I am working on TC29X controller. Unfortunately boot mode headers are erased and I am unable to flash through lauterbcah. I am trying to use miniwiggler and I have connected target using 10 pin DAP connector to miniwiggler. But when I run DAS sevice scanner I see "No Device(DAS JDS miniWiggler V3.1)" message. Can anyone please help me ?

Thanks,
Gayathri
0 Likes
This widget could not be displayed.