Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

User7559
Level 2
Level 2
5 sign-ins First like received 10 questions asked
I want to use the Data Access Overlay(OVC) function with TC233.

Can you provide material or example source for this function?
4 Replies
NeMa_4793301
Level 6
Level 6
10 likes received 10 solutions authored 5 solutions authored
Here is a little example of overlay. I wrote it for a TC27x, so it's using OVC2 (CPU2 overlay registers) instead of OVC0, and it remaps PFLASH access to LMU RAM, so you'll need to adapt the addresses to your use case.

/*****************************************************
*
* TC27x_overlay.c
*
* Description : Demo of overlay memory
*
*/

#include

typedef unsigned long U32;

#pragma align 32
const U32 Test_Map_Cal_Flash[32] = {0,1,2,3,4,5,6,7,8,9,0,1,2,3,4,5,6,7,8,9,0,1,2,3,4,5,6,7,8,9,0,1};
#pragma align restore

#pragma align 32
volatile U32 Test_Map_Cal_Ram[32] = {9,19,29,93,49,59,96,79,98,99,90,91,92,93,94,95,96,97,98,99,90,91,92,93,94,95,96,97,98,99,90,91};
#pragma align restore

U32 *lmu_ptr;

#pragma align 32
volatile U32 Test_Algo_Update[32];
#pragma align restore

OVC0_RABR0_type rabr =
{
.B.OMEM=6, // Overlay Memory Select: Redirection to Core 2 DSPR !*!*!* make sure that's true!
.B.OVEN=1 // Overlay enabled
};

OVC0_OTAR0_type otar;

const OVC0_OMASK0_type omask =
{
// .B.OMASK = 0xFFF // Overlay Address Mask: 32 byte block size
.B.OMASK = 0xE00 // Overlay Address Mask: 1024 byte block size
};

const OVC0_OSEL_type osel =
{
.B.SHOVEN0 = 1 // Shadow Overlay Enable 0: overlay block 0 is enabled
};

const SCU_OVCENABLE_type ovcenable =
{
.B.OVEN2 = 1 // Overlay Enable 0: OVC is enabled on CPU2
};

const SCU_OVCCON_type ovccon =
{
.B.CSEL2 = 1, // CPU Select 0
.B.OVSTRT = 1, // Overlay Start
.B.DCINVAL = 1, // Data Cache Invalidate
.B.OVCONF = 1 // Overlay Configured
};

int main(void)
{
for( ;; )
{
}
}

int main2(void)
{
int i;

lmu_ptr = (U32 *) 0xB0004000;
for( i=0; i<31; i++ )
{
lmu_ptr = Test_Map_Cal_Ram;
}


// Configure the details for overlay memory
// - remap Test_Map_Cal_Flash reads into Test_Map_Cal_Ram
// - this is making gross assumptions that Test_Map_Cal_Ram is in CPU2's DSPR
//
_endinit_clear();
rabr.B.OBASE = ( (unsigned long) (lmu_ptr) >> 5) & 0x1FFFF;
OVC2_RABR0.U = rabr.U;
otar.B.TBASE= ( (unsigned long) (&Test_Map_Cal_Flash) >> 5) & 0x7FFFF;
OVC2_OTAR0.U = otar.U;
OVC2_OMASK0.U = omask.U;
OVC2_OSEL.U = osel.U;
_endinit_set();

_safety_endinit_clear();
SCU_OVCENABLE.U = ovcenable.U;
_safety_endinit_set();

SCU_OVCCON.U = ovccon.U; // Turn on overlay memory

__dsync();

// Now copy Test_Map_Cal_Flash into Test_Algo_Update
// - CPU0 reads from Test_Map_Cal_Flash will instead read from Test_Map_Cal_Ram
// - note that the debugger bypasses the overlay system, so it can't be fooled
//
for( i=0; i<31; i++ )
{
Test_Algo_Update = Test_Map_Cal_Flash;
}

for( ;; )
{
}
}
User22480
Level 1
Level 1
Hi, UC_wrangler.

Thanks for sharing on the Overlay sample code, I tested it works, but somehow it is kind of "overlay RAM is updated once" only.
Basically, I just want to have a live overlay RAM update, so I put the Test_Algo_Update in the infinite loop (see code below).

But somehow, after Test_Algo_Update[] is updated, then I go and update the 0xB0004000 in Lauterbach debugger, but I don't see Test_Algo_Update[] is updated.... Why?
Any idea?

int main2(void)
{
:
:


for( ;; )
{
for( i=0; i<31; i++ )
{
Test_Algo_Update = Test_Map_Cal_Flash;
}
}
}

Thanks and regards,
William.
0 Likes
NeMa_4793301
Level 6
Level 6
10 likes received 10 solutions authored 5 solutions authored
Overlay is a per-CPU feature; when you view a debugger window, it doesn't include overlay.

In Lauterbach, try doing SYStem.Option OVC ON, to force the debugger to use the CPU's point of view.
NXTY_Ota
Level 3
Level 3
25 sign-ins 10 replies posted First like received

I could not make OVC executed on TC39x by simply copying the code described in this topic, so I created a PJ that executes OVC the TC39x using AURIX™ Development Studio and have attached it.

To make it executed on other than TC39x, please copy Cpu0_Main.c, Cpu2_Main.c, and Cpu2_Main.h to a PJ of the family you would like to make OVC executed on.

0 Likes
This widget could not be displayed.