Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
SWYoon
Level 2
Level 2
Distributor - Changnam (South Korea)
25 sign-ins 10 sign-ins 5 sign-ins
I want to use the Data Access Overlay(OVC) function with TC233.

Can you provide material or example source for this function?
4 Replies
NeMa_4793301
Level 6
Level 6
10 likes received 10 solutions authored 5 solutions authored
Here is a little example of overlay. I wrote it for a TC27x, so it's using OVC2 (CPU2 overlay registers) instead of OVC0, and it remaps PFLASH access to LMU RAM, so you'll need to adapt the addresses to your use case.

/*****************************************************
*
* TC27x_overlay.c
*
* Description : Demo of overlay memory
*
*/

#include

typedef unsigned long U32;

#pragma align 32
const U32 Test_Map_Cal_Flash[32] = {0,1,2,3,4,5,6,7,8,9,0,1,2,3,4,5,6,7,8,9,0,1,2,3,4,5,6,7,8,9,0,1};
#pragma align restore

#pragma align 32
volatile U32 Test_Map_Cal_Ram[32] = {9,19,29,93,49,59,96,79,98,99,90,91,92,93,94,95,96,97,98,99,90,91,92,93,94,95,96,97,98,99,90,91};
#pragma align restore

U32 *lmu_ptr;

#pragma align 32
volatile U32 Test_Algo_Update[32];
#pragma align restore

OVC0_RABR0_type rabr =
{
.B.OMEM=6, // Overlay Memory Select: Redirection to Core 2 DSPR !*!*!* make sure that's true!
.B.OVEN=1 // Overlay enabled
};

OVC0_OTAR0_type otar;

const OVC0_OMASK0_type omask =
{
// .B.OMASK = 0xFFF // Overlay Address Mask: 32 byte block size
.B.OMASK = 0xE00 // Overlay Address Mask: 1024 byte block size
};

const OVC0_OSEL_type osel =
{
.B.SHOVEN0 = 1 // Shadow Overlay Enable 0: overlay block 0 is enabled
};

const SCU_OVCENABLE_type ovcenable =
{
.B.OVEN2 = 1 // Overlay Enable 0: OVC is enabled on CPU2
};

const SCU_OVCCON_type ovccon =
{
.B.CSEL2 = 1, // CPU Select 0
.B.OVSTRT = 1, // Overlay Start
.B.DCINVAL = 1, // Data Cache Invalidate
.B.OVCONF = 1 // Overlay Configured
};

int main(void)
{
for( ;; )
{
}
}

int main2(void)
{
int i;

lmu_ptr = (U32 *) 0xB0004000;
for( i=0; i<31; i++ )
{
lmu_ptr = Test_Map_Cal_Ram;
}


// Configure the details for overlay memory
// - remap Test_Map_Cal_Flash reads into Test_Map_Cal_Ram
// - this is making gross assumptions that Test_Map_Cal_Ram is in CPU2's DSPR
//
_endinit_clear();
rabr.B.OBASE = ( (unsigned long) (lmu_ptr) >> 5) & 0x1FFFF;
OVC2_RABR0.U = rabr.U;
otar.B.TBASE= ( (unsigned long) (&Test_Map_Cal_Flash) >> 5) & 0x7FFFF;
OVC2_OTAR0.U = otar.U;
OVC2_OMASK0.U = omask.U;
OVC2_OSEL.U = osel.U;
_endinit_set();

_safety_endinit_clear();
SCU_OVCENABLE.U = ovcenable.U;
_safety_endinit_set();

SCU_OVCCON.U = ovccon.U; // Turn on overlay memory

__dsync();

// Now copy Test_Map_Cal_Flash into Test_Algo_Update
// - CPU0 reads from Test_Map_Cal_Flash will instead read from Test_Map_Cal_Ram
// - note that the debugger bypasses the overlay system, so it can't be fooled
//
for( i=0; i<31; i++ )
{
Test_Algo_Update = Test_Map_Cal_Flash;
}

for( ;; )
{
}
}
User22480
Level 1
Level 1
Hi, UC_wrangler.

Thanks for sharing on the Overlay sample code, I tested it works, but somehow it is kind of "overlay RAM is updated once" only.
Basically, I just want to have a live overlay RAM update, so I put the Test_Algo_Update in the infinite loop (see code below).

But somehow, after Test_Algo_Update[] is updated, then I go and update the 0xB0004000 in Lauterbach debugger, but I don't see Test_Algo_Update[] is updated.... Why?
Any idea?

int main2(void)
{
:
:


for( ;; )
{
for( i=0; i<31; i++ )
{
Test_Algo_Update = Test_Map_Cal_Flash;
}
}
}

Thanks and regards,
William.
0 Likes
NeMa_4793301
Level 6
Level 6
10 likes received 10 solutions authored 5 solutions authored
Overlay is a per-CPU feature; when you view a debugger window, it doesn't include overlay.

In Lauterbach, try doing SYStem.Option OVC ON, to force the debugger to use the CPU's point of view.
lock attach
Attachments are accessible only for community members.
NXTY_Ota
Level 4
Level 4
Distributor - NEXTY (Japan)
100 sign-ins 10 likes given 5 likes given

I could not make OVC executed on TC39x by simply copying the code described in this topic, so I created a PJ that executes OVC the TC39x using AURIX™ Development Studio and have attached it.

To make it executed on other than TC39x, please copy Cpu0_Main.c, Cpu2_Main.c, and Cpu2_Main.h to a PJ of the family you would like to make OVC executed on.