Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

TeeEff
Level 1
Level 1
First like received 5 sign-ins First reply posted

Hello,

I'm confused with the TC2x Data Sheet where we could read :

Data Flash Endurance per EEPROMx sector (NE_EEP10 C): 125 000 cycles Min 

and 

Number of erase operations on DF0 over lifetime (NERD0 CC): 750 000 cycles Max

I did not really understand the difference between these two values.

Does it means that if the 12 sectors are used evenly distributed, the maximum cycles for each sector is 62 500 cycles Max (750 000 / 12) ?

 

0 Likes
2 Replies
Prudhvi
Moderator
Moderator
Moderator
25 likes received 50 solutions authored 250 sign-ins

Hi,

DF0 contains both EEPROM & UCB. I've taken TC29x as reference and tried to answer your queries below:

                                           Prudhvi_0-1652265120068.png

The value of 125000 cycles is the minimum value for Data Flash Endurance (P/E) per EEPROMx sector with max retention of 10 years. We have 96 EEPROM sectors in TC29x as shown in the above image.

The Number of erase operations on DF0 (complete) over lifetime is 750000 cycles and this is maximum value.

Regards,

Prudhvi.

0 Likes
TeeEff
Level 1
Level 1
First like received 5 sign-ins First reply posted

Thanks you Prudhvi.

 

How are computed the erase operations ? If several sectors are requested to be erased, this is counted as one operation or counted as the number of sector ?

 

Regards

0 Likes