Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
wangjiajie
Level 1
Level 1
First question asked Welcome!

上午能连,下午重新插拔了一下就一直连不上了,一个绿灯能够长亮,另一个绿灯一闪一闪的。

 

Device No Device connected
Device ID0 is 0x00000000
Device ID1 is 0x00000000
Valid Address Maps: None

Connected over DAS Server
Name: UDAS
Provider: Infineon
Release V3.10 (Aug 27 2019) based on
Server library V3.0 and DAS API V4.1
Host address "localhost" on port 49788
Process ID 6448
Server provides these ports:
DummyDevice 1 instances
DAP/JTAG/SPD/SWD 16 instances

Using DAP/JTAG/SPD/SWD port 0

Access Hardware
Name: DAS JDS miniWiggler V3.1
Provider: Infineon
Serial Number: MW5Y8JLU
Active Interface: JTAG

0 Likes
1 Reply
Di_W
Moderator
Moderator
Moderator
1000 replies posted 250 solutions authored 100 likes received

可以换一个Triboard试试,或者换一个PC试试。

0 Likes