Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

Prethveraj
Level 1
First reply posted First question asked Welcome!
Level 1

AurixFlasher - DAS::Error: Device reset could not be performed.
Overall time: 732 ms
AurixFlasher Exit Status: Fail

 

What does this error means? The code for reading single channel through ADC is able to flash. But this error occurred when I tried to flash the code to read multiple input voltage through ADC.  The code have 0 error, but can't flash. How to solve this issue?

It's not a Hardware issue since I can flash other programs.

0 Likes
2 Replies
Nambi
Moderator
Moderator 250 sign-ins 100 replies posted 10 likes received
Moderator
0 Likes
Prethveraj
Level 1
First reply posted First question asked Welcome!
Level 1

Hi,

Thank you for your reply.

I checked that solution before I posted this error.

It's not a hardware error. I have several codes running on the microcontroller TC233lp and some doesn't flash and gives this error. So it is software error. Do you have any idea what causes the error? 

0 Likes