Aug 14, 2019
04:29 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Aug 14, 2019
04:29 AM
Hi,
to programming my TC233LP-32F200N i would like to use the DAP interface. I bought a miniWiggler V3.1 for that and I read the manual of the TriBoard TC233 for the wiring.The wiring result is the picture below!

I had a board made for this purpose.
It´s only a try to check the DAP interface, but it doesn´t works. I dont can connect to my prozessor. The settings of the InfineonMemTool are correct and the miniWiggler works, because i tested it successfully on the TriBoard TC233 V1.1.
Did I forget anything on the board, or is the wiring wrong??
Thanks for help
to programming my TC233LP-32F200N i would like to use the DAP interface. I bought a miniWiggler V3.1 for that and I read the manual of the TriBoard TC233 for the wiring.The wiring result is the picture below!
I had a board made for this purpose.
It´s only a try to check the DAP interface, but it doesn´t works. I dont can connect to my prozessor. The settings of the InfineonMemTool are correct and the miniWiggler works, because i tested it successfully on the TriBoard TC233 V1.1.
Did I forget anything on the board, or is the wiring wrong??
Thanks for help
- Tags:
- IFX
2 Replies
Aug 16, 2019
06:54 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Aug 16, 2019
06:54 AM
As long as PORST signal is low, the DAP Interface is not working,
There is missing an external pull-up (1K ~ 2K2) on PORST. PORST has internal pull-down which is always active. Therefore the PORST is always low without an external pull-up
There is missing an external pull-up (1K ~ 2K2) on PORST. PORST has internal pull-down which is always active. Therefore the PORST is always low without an external pull-up
Aug 19, 2019
04:35 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Aug 19, 2019
04:35 AM
Thank you for your help! I´ll give it a try
This widget could not be displayed.