Jul 16, 2021
07:14 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jul 16, 2021
07:14 AM
Hi everyone!
I have been trying to create 3 complementary pairs of PWM outputs with a high and low channel using the IfxGtm_Atom_PwmHl driver. The functionalities I need are deadtime and shifted output.
Before, I managed to create 3 complementary pairs of PWM output with deadtime using the CCU6 library, but since I also need to be able to shift the output relative to other channels, I believe this module is not suited anymore.
Thus, I land at the IfxGtm_Atom_PwmHl driver. Sadly, I can not generate PWM outputs at all. Can someone point me in the right direction?
Using only IfxGtm_Atom_PwmHl
Using standard interface:
Alternatively, the full source is attached.
I have been trying to create 3 complementary pairs of PWM outputs with a high and low channel using the IfxGtm_Atom_PwmHl driver. The functionalities I need are deadtime and shifted output.
Before, I managed to create 3 complementary pairs of PWM output with deadtime using the CCU6 library, but since I also need to be able to shift the output relative to other channels, I believe this module is not suited anymore.
Thus, I land at the IfxGtm_Atom_PwmHl driver. Sadly, I can not generate PWM outputs at all. Can someone point me in the right direction?
Using only IfxGtm_Atom_PwmHl
#include "Ifx_Types.h"
#include "IfxGtm_Atom_PwmHl.h"
// #include "IfxGtm_Atom_Dtm_PwmHl.h"
#include "PWM_Atom.h"
// Configuration
#define FXUCLK_FREQUENCY 100e6 // FXU Clock base frequency, in Hertz
#define PWM_FREQUENCY 105e3 // PWM signal frequency, in Hertz
#define PWM_PERIOD (FXUCLK_FREQUENCY / PWM_FREQUENCY) // PWM signal period, in ticks
//#define DEADTIME 200e-9 // Dead time in seconds - 200 ns. When an
// unexpected deadtime of 2.55e-x occurs,
// the deadtime is bigger than allowed.
#define NUMBER_OF_CHANNELS 1
void init_stdif_pwmhl(void)
{
// prepare ccx coutx in advance
IfxGtm_Atom_ToutMapP ccx[NUMBER_OF_CHANNELS];
IfxGtm_Atom_ToutMapP coutx[NUMBER_OF_CHANNELS];
ccx[0] = &IfxGtm_ATOM0_0_TOUT0_P02_0_OUT;
coutx[0] = &IfxGtm_ATOM0_1_TOUT1_P02_1_OUT;
// init
// - clock
IfxGtm_enable(&MODULE_GTM); /* Enable GTM */
IfxGtm_Cmu_enableClocks(&MODULE_GTM, IFXGTM_CMU_CLKEN_FXCLK); /* Enable the FXU clock */
// - timer
IfxGtm_Atom_Timer timer;
IfxGtm_Atom_Timer_Config timerConfig;
IfxGtm_Atom_Timer_initConfig(&timerConfig, &MODULE_GTM);
// g_atomConfig.pin.outputPin = &LED; /* Set LED as output */
// g_atomConfig.synchronousUpdateEnabled = TRUE; /* Enable synchronous update */
timerConfig.atom = ccx[0]->atom;
timerConfig.timerChannel = ccx[0]->channel; // but the channel of coutx[0] is also used! How to tell the driver?
// timerConfig.initPins = FALSE; // No idea what to use
timerConfig.base.frequency = PWM_FREQUENCY;
timerConfig.base.countDir = IfxStdIf_Timer_CountDir_up;
// timerConfig.base.trigger.enabled = TRUE; // 1/2 IfxCpu_Trap_busError
// timerConfig.base.trigger.outputEnabled = TRUE; // 2/2 IfxCpu_Trap_busError
IfxGtm_Atom_Timer_init(&timer, &timerConfig);
IfxGtm_Atom_Timer_run(&timer);
// - pwmHl
// IfxGtm_AtomDtm_PwmHl pwmHl;
// IfxGtm_Atom_Dtm_PwmHl_Config pwmHlConfig;
// IfxGtm_Atom_Dtm_PwmHl_initConfig(&pwmHlConfig);
IfxGtm_Atom_PwmHl pwmHl;
IfxGtm_Atom_PwmHl_Config pwmHlConfig;
IfxGtm_Atom_PwmHl_initConfig(&pwmHlConfig);
// pwmHlConfig.base.deadtime = 200e-9;
// pwmHlConfig.base.minPulse = 100e-9;
pwmHlConfig.base.channelCount = NUMBER_OF_CHANNELS;
// pwmHlConfig.base.emergencyEnabled = FALSE;
pwmHlConfig.base.outputMode = IfxPort_OutputMode_pushPull;
pwmHlConfig.base.outputDriver = IfxPort_PadDriver_cmosAutomotiveSpeed3;
pwmHlConfig.base.ccxOutputEnabled = TRUE;
pwmHlConfig.base.coutxOutputEnabled = TRUE;
// pwmHlConfig.base.ccxActiveState = Ifx_ActiveState_high;
// pwmHlConfig.base.coutxActiveState = Ifx_ActiveState_high;
// ccx and coutx configuration moved upwards
pwmHlConfig.timer = &timer;
pwmHlConfig.atom = timer.atomIndex;
pwmHlConfig.ccx = ccx;
pwmHlConfig.coutx = coutx;
// IfxGtm_Atom_Dtm_PwmHl_init(&pwmHl, &pwmHlConfig);
// IfxGtm_Atom_Dtm_PwmHl_setMode(&pwmHl, Ifx_Pwm_Mode_leftAligned);
IfxGtm_Atom_PwmHl_init(&pwmHl, &pwmHlConfig);
IfxGtm_Atom_PwmHl_setMode(&pwmHl, Ifx_Pwm_Mode_leftAligned);
// run
IfxGtm_Atom_Timer_run(&timer);
IfxGtm_Atom_Timer_disableUpdate(&timer);
IfxGtm_Atom_Timer_setSingleMode(&timer, FALSE);
IfxGtm_Atom_Timer_applyUpdate(&timer);
Ifx_TimerValue tOn = (uint32) PWM_PERIOD/2;
// Ifx_TimerValue tOn[2] = {PWM_PERIOD/2, PWM_PERIOD/2};
IfxGtm_Atom_PwmHl_setOnTime(&pwmHl, &tOn);
}
Using standard interface:
#include "Ifx_Types.h"
#include "IfxGtm_Atom_PwmHl.h"
// #include "IfxGtm_Atom_Dtm_PwmHl.h"
#include "PWM_Atom.h"
// Configuration
#define FXUCLK_FREQUENCY 100e6 // FXU Clock base frequency, in Hertz
#define PWM_FREQUENCY 105e3 // PWM signal frequency, in Hertz
#define PWM_PERIOD (FXUCLK_FREQUENCY / PWM_FREQUENCY) // PWM signal period, in ticks
//#define DEADTIME 200e-9 // Dead time in seconds - 200 ns. When an
// unexpected deadtime of 2.55e-x occurs,
// the deadtime is bigger than allowed.
#define NUMBER_OF_CHANNELS 1
void init_stdif_pwmhl(void)
{
// prepare ccx coutx in advance
IfxGtm_Atom_ToutMapP ccx[NUMBER_OF_CHANNELS];
IfxGtm_Atom_ToutMapP coutx[NUMBER_OF_CHANNELS];
ccx[0] = &IfxGtm_ATOM0_0_TOUT0_P02_0_OUT;
coutx[0] = &IfxGtm_ATOM0_1_TOUT1_P02_1_OUT;
// init
// - clock
IfxGtm_enable(&MODULE_GTM); /* Enable GTM */
IfxGtm_Cmu_enableClocks(&MODULE_GTM, IFXGTM_CMU_CLKEN_FXCLK); /* Enable the FXU clock */
// - timer
IfxGtm_Atom_Timer timer;
IfxGtm_Atom_Timer_Config timerConfig;
IfxGtm_Atom_Timer_initConfig(&timerConfig, &MODULE_GTM);
// g_atomConfig.pin.outputPin = &LED; /* Set LED as output */
// g_atomConfig.synchronousUpdateEnabled = TRUE; /* Enable synchronous update */
timerConfig.atom = ccx[0]->atom;
timerConfig.timerChannel = ccx[0]->channel; // but the channel of coutx[0] is also used! How to tell the driver?
// timerConfig.initPins = FALSE; // No idea what to use
timerConfig.base.frequency = PWM_FREQUENCY;
timerConfig.base.countDir = IfxStdIf_Timer_CountDir_up;
// timerConfig.base.trigger.enabled = TRUE; // 1/2 IfxCpu_Trap_busError
// timerConfig.base.trigger.outputEnabled = TRUE; // 2/2 IfxCpu_Trap_busError
IfxGtm_Atom_Timer_init(&timer, &timerConfig);
IfxGtm_Atom_Timer_run(&timer);
// - pwmHl
// IfxGtm_AtomDtm_PwmHl pwmHl;
// IfxGtm_Atom_Dtm_PwmHl_Config pwmHlConfig;
// IfxGtm_Atom_Dtm_PwmHl_initConfig(&pwmHlConfig);
IfxGtm_Atom_PwmHl pwmHl;
IfxGtm_Atom_PwmHl_Config pwmHlConfig;
IfxGtm_Atom_PwmHl_initConfig(&pwmHlConfig);
// pwmHlConfig.base.deadtime = 200e-9;
// pwmHlConfig.base.minPulse = 100e-9;
pwmHlConfig.base.channelCount = NUMBER_OF_CHANNELS;
// pwmHlConfig.base.emergencyEnabled = FALSE;
pwmHlConfig.base.outputMode = IfxPort_OutputMode_pushPull;
pwmHlConfig.base.outputDriver = IfxPort_PadDriver_cmosAutomotiveSpeed3;
pwmHlConfig.base.ccxOutputEnabled = TRUE;
pwmHlConfig.base.coutxOutputEnabled = TRUE;
// pwmHlConfig.base.ccxActiveState = Ifx_ActiveState_high;
// pwmHlConfig.base.coutxActiveState = Ifx_ActiveState_high;
// ccx and coutx configuration moved upwards
pwmHlConfig.timer = &timer;
pwmHlConfig.atom = timer.atomIndex;
pwmHlConfig.ccx = ccx;
pwmHlConfig.coutx = coutx;
// IfxGtm_Atom_Dtm_PwmHl_init(&pwmHl, &pwmHlConfig);
// IfxGtm_Atom_Dtm_PwmHl_setMode(&pwmHl, Ifx_Pwm_Mode_leftAligned);
IfxGtm_Atom_PwmHl_init(&pwmHl, &pwmHlConfig);
IfxGtm_Atom_PwmHl_setMode(&pwmHl, Ifx_Pwm_Mode_leftAligned);
// run
// - setup stdif
IfxStdIf_Timer timer_stdif;
IfxGtm_Atom_Timer_stdIfTimerInit(&timer_stdif, &timer);
// IfxStdIf_Timer *timer_stdif = IfxStdIf_PwmHl_getTimer(&pwmHl_stdif);
IfxStdIf_PwmHl pwmHl_stdif;
IfxGtm_Atom_Dtm_PwmHl_stdIfPwmHlInit(&pwmHl_stdif, &pwmHl);
// - run stdif
IfxStdIf_Timer_run(&timer_stdif);
IfxStdIf_Timer_disableUpdate(&timer_stdif); // To allow timer changes
Ifx_TimerValue tOn = (uint32) PWM_PERIOD/2;
// Set trigger point
// IfxStdIf_Timer_setTrigger(&timer_stdif, tOn);
// Set period of cycle
Ifx_TimerValue period = (uint32) PWM_PERIOD;
IfxStdIf_Timer_setPeriod(&timer_stdif, period);
// Set duty cycle on time
IfxStdIf_PwmHl_setOnTime(&pwmHl_stdif, &tOn);
IfxStdIf_Timer_applyUpdate(&timer_stdif); // To implement timer changes
IfxStdIf_Timer_run(&timer_stdif);
}
Alternatively, the full source is attached.
Solved! Go to Solution.
1 Solution
Jul 30, 2021
02:35 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jul 30, 2021
02:35 AM
For anyone trying themselves, I've uploaded an example project to learn from.
1. It uses a PWM timer channel for the counter reset in PWM output channels (IfxGtm_Atom_Timer),
2. allows to set phase-shifted signals in PWM output channels (IfxGtm_Atom_Pwm),
3. uses the deadtime module to create complementary signals with deadtime between the signals from the PWM output channels (IfxGtm_Atom_Dtm_PwmHl),
4. uses on-board LEDs for visual debugging.
The pins are configured for the TC367.
Good luck with your goal!
1. It uses a PWM timer channel for the counter reset in PWM output channels (IfxGtm_Atom_Timer),
2. allows to set phase-shifted signals in PWM output channels (IfxGtm_Atom_Pwm),
3. uses the deadtime module to create complementary signals with deadtime between the signals from the PWM output channels (IfxGtm_Atom_Dtm_PwmHl),
4. uses on-board LEDs for visual debugging.
The pins are configured for the TC367.
Good luck with your goal!
4 Replies
Jul 18, 2021
11:30 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jul 18, 2021
11:30 PM
Hello,
did you try using one of the trainings for GTM? I believe you have the TC367 device, therefore this should be fine for you: GTM_TOM_PWM_1_KIT_TC367_TFT with its tutorial
there are more trainings for GTM, you can search them with AURIX Development Studio when you import an AURIX project.
did you try using one of the trainings for GTM? I believe you have the TC367 device, therefore this should be fine for you: GTM_TOM_PWM_1_KIT_TC367_TFT with its tutorial
there are more trainings for GTM, you can search them with AURIX Development Studio when you import an AURIX project.
Jul 19, 2021
12:00 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jul 19, 2021
12:00 AM
Hi teoBits, thanks for your response.
I have indeed tried the GTM_TOM_PWM_1_KIT_TC367_TFT tutorial, but sadly it only allowed me to set the frequency of a module and the duty cycle of a channel.
I based my work partly on this tutorial, but since I also need complementary channels, deadtime and a shifted output between different channels, this tutorial did not suffice for me.
Do you know of a tutorial which does this all? I believe there are none, sadly, so I was trying to create my own work using the iLLD documentation.
I have indeed tried the GTM_TOM_PWM_1_KIT_TC367_TFT tutorial, but sadly it only allowed me to set the frequency of a module and the duty cycle of a channel.
I based my work partly on this tutorial, but since I also need complementary channels, deadtime and a shifted output between different channels, this tutorial did not suffice for me.
Do you know of a tutorial which does this all? I believe there are none, sadly, so I was trying to create my own work using the iLLD documentation.
Jul 19, 2021
12:47 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jul 19, 2021
12:47 AM
Perhaps Application Note AP32356, PWMAC (PWM Master of AC motor) would help, but we could not find the location of the project (GLT_PWMMAC_TC39x_golden). Could you provide us with a link toward myicp containing the project folder?
Jul 30, 2021
02:35 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jul 30, 2021
02:35 AM
For anyone trying themselves, I've uploaded an example project to learn from.
1. It uses a PWM timer channel for the counter reset in PWM output channels (IfxGtm_Atom_Timer),
2. allows to set phase-shifted signals in PWM output channels (IfxGtm_Atom_Pwm),
3. uses the deadtime module to create complementary signals with deadtime between the signals from the PWM output channels (IfxGtm_Atom_Dtm_PwmHl),
4. uses on-board LEDs for visual debugging.
The pins are configured for the TC367.
Good luck with your goal!
1. It uses a PWM timer channel for the counter reset in PWM output channels (IfxGtm_Atom_Timer),
2. allows to set phase-shifted signals in PWM output channels (IfxGtm_Atom_Pwm),
3. uses the deadtime module to create complementary signals with deadtime between the signals from the PWM output channels (IfxGtm_Atom_Dtm_PwmHl),
4. uses on-board LEDs for visual debugging.
The pins are configured for the TC367.
Good luck with your goal!