Unfortunately it was not possible for me to fully get behind how the Aurix Development Studio configures the flash target in an existing project.
Therefore, I ended up using other tools than the Aurix Development Studio, which in my case are command line utilities in combination with VS Code.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Lucas, if you first trial ETH_LWIP project, please note that it is old-styled build using BIFACES. To use BIFACES, you could download from myICP and configure the compiler PATH, which supports Tasking/Hightec/Greenhills/Windriver. You can use Tasking compiler (evaluation or commercial version) as a start. Once you installed BIFACES and configured proper compiler in .xml file, then you can try to build the whole project.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
thanks for pointing out that BIFACES is the old-style build environment. I chose the project because it is, to my knowledge, the only FreeRTOS sample project readily available for the Tricore.
For clarification, I have set up the build toolchain successfully and can build the project which generates a valid .elf binary. I can even flash the binary, but I must do so manually.
How can I configure the built-in flash option to just run Aurix Flasher with the generated .elf binary? Something is going wrong when I click the flash button but I don't get any console output.
Best,
Lukas
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
Unfortunately it was not possible for me to fully get behind how the Aurix Development Studio configures the flash target in an existing project.
Therefore, I ended up using other tools than the Aurix Development Studio, which in my case are command line utilities in combination with VS Code.