Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

Kumaresh
Level 3
Level 3
10 questions asked 10 replies posted First solution authored
Hi ,
Background : We transfer 12bit Single Channel ADC data over DMA and want to compute CRC using our SW and compare it with the checksum computed by the DMA. For our SW computation we use FCE to calculate CRC.
Problem :
Lets say the data we transferred by DMA = 0x804
DMA computed checksum = 0x8E6D5CEE
 
When I use FCE to compute the CRC the Input data is always taken in 32 bit format i.e 0x00 0x00 0x08 0x04.
And the CRC I get for this is 0xEEF0910D
 
Both the CRC's are correct the only difference is the input data format.
Question : Is it possible to use FCE to calculate CRC-32 for a 16 bit data ? If so could you please assist me on this.
Screenshot : 
 
Kumaresh_1-1674378387995.png

 

 
Note : Changed DMA data transfer width to 32 bit and CRC computation is okay. But as we use only one ADC channel that other half contains some garbage data. 
 
Thanks,
Kumaresh
0 Likes
5 Replies
Aiswarya
Moderator
Moderator
Moderator
25 solutions authored 50 replies posted 100 sign-ins

Hi,

In FCE, the bit width of each word should be in terms of KERNEL polynomial width.
You would need to pad the 16-bit data.

Please find the thread below:
https://community.infineon.com/t5/AURIX/Calculated-CRC-from-FCE-on-the-DMA-data-being-transferred-do...

Regards,
Aiswarya.

0 Likes

Hi, If I pad other 16 bits to the data which I need to calculate CRC using FCE then it will be different by the CRC calculated by DMA.  Does the padded bits also considered in CRC calculation? From my testing I see that the CRC is computed with padded bits. So thought to confirm with you

0 Likes
µC_Wrangler
Employee
Employee
100 sign-ins 25 likes received 25 solutions authored

Hi Kumaresh.  Is this for TC2xx?  If so, the incorrect value in DMA RDCRC for 8- and 16-bit transfers is a known issue - see DMA_TC.039 in the errata sheet.  The erratum was fixed in TC3xx.

DMA_TC.039 Read Data CRC
The Read Data CRC (RDCRC) calculates an IEEE 802.3 ethernet CRC32 checksum as DMA moves read data through the DMA. The DMA implementation of the algorithm does not zero extend the read data for SDTB (8-bit) and SDTH (16-bit) accesses resulting in the calculation of a wrong checksum value.

The RDCRC must only be used with STDW (32-bit), SDTD (64-bit), BTR2 (128-bit) and BTR4 (256-bit) access sizes. It must be noted that SDTD, BTR2 and BTR4 are only supported for SRI-source to SRI-destination transactions.

0 Likes

Hi, I observe this behaviour in TC377

0 Likes
Aiswarya
Moderator
Moderator
Moderator
25 solutions authored 50 replies posted 100 sign-ins

Hello, 

Could you please share the complete data stream fed to DMA and the FCE engine?

 

Kind Regards,
Aiswarya.

0 Likes