- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
How to configure port routing?:
- Infineon sample leaves the part open: Line 159 in IfxEdsadc_Edsadc.c
- tutorial EDSADC_1 for KIT_AURIX_TC375_LK mentions channel 3 and port pin AN0 - i do not see it in the code implementation
- where to look in the docu for this topic?
With register GLOBRC i start EDSADC module run:
- how do i check if it is running?
- and if it is running not/properly?
EDSADC module has many setting options:
- which are the important one?
- important for basic functionality?
Thanks for your support
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
In TC37X_ts_appx_v2.5.1.pdf 33.3.1 Analog Module Connections, You will see there are 6 channel EDS0-EDS5, which can connect Source Pins. For No.3 channel, INMUX bitfield will select AN0/AN1/AN14/AN15.
In 33.3.2 Digital Module Connections, you will see other connections which is specific for diginal.
The trigger input line is selected via bitfield TRSEL = [yyyyB], the data input line (DSDIN…) is selected via bitfield DSRCEX = [yyyB], the clock input line (DSCIN…) is selected via bitfield CSRCEX = [yyyB].
1.You can apply access for MyICP:
2. Folder of 37x tech specs:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
In TC37X_ts_appx_v2.5.1.pdf 33.3.1 Analog Module Connections, You will see there are 6 channel EDS0-EDS5, which can connect Source Pins. For No.3 channel, INMUX bitfield will select AN0/AN1/AN14/AN15.
In 33.3.2 Digital Module Connections, you will see other connections which is specific for diginal.
The trigger input line is selected via bitfield TRSEL = [yyyyB], the data input line (DSDIN…) is selected via bitfield DSRCEX = [yyyB], the clock input line (DSCIN…) is selected via bitfield CSRCEX = [yyyB].
1.You can apply access for MyICP:
2. Folder of 37x tech specs: