- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi all
I'm trying to relocate some variable from one core to the other using
#pragma data_core_association private0/1/2
I notice that the variable is moved from dsram to psram there is a way to decide where to relocate the variable?
e.g.
static uint32_t bar; -> bar located into dsram0
#pragma data_core_association private0
static uint32_t bar; -> bar located into psram0
#pragma data_core_association restore
Thanks
Solved! Go to Solution.
- Labels:
-
AURIX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi FD,
I have asked for internal team and perhaps this is needed to ask compiler tech support, please notice that the Tasking free toolchain's support is limited. However you could use the workaround first.
Besides, there is a PSPR code sample for your reference:
//_____________________________Locate test for CPU0 related pspr code_________________________________
#if defined(__TASKING__)
#pragma section code "psram_text_cpu0"
#elif defined(__GNUC__)
#pragma section ".psram_text_cpu0" axw
#elif defined(__DCC__)
#pragma section CODE ".psram_text_cpu0" standard RXW
#elif defined(__ghs__)
#pragma ghs section text=".psram_text_cpu0"
#endif
uint32 Locate_PsprCode_fc0(void)
{
return retData0;
}
#if defined(__GNUC__)
#pragma section
#endif
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi FD_aurix,
I have found an example from https://github.com/Infineon/AURIX_code_examples/blob/288e353e583148009bd03c16d65db76370cba1af/code_e...
You could check if .lsl file has some section names you could use.
Above is for your reference.
Or you can check the compiler's user manual for details. i.e.https://www.tasking.com/support/tricore/ctc_user_guide_v6.3r1.pdf
dw
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi dw
Thanks for the reply.
I've checked the manual and the private memory qualifier should "Preferably in core n local RAM. If the memory is full, other memory is used." But it is not specified what is the "local RAM" and for sure the DSRAM of this core is not full 😄
in the example it is used the #pragma section that seems only a renaming features
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Dear Users,
Please refer to below link, I have tried DLMU0-5/ DSPR0-5/ and LMU.
Note that edmem and psram I have not tried.
You can use the same way to your application. The .lsl file is attached.
https://community.infineon.com/t5/AURIX/Unable-to-read-write-to-DLMU/m-p/346011/highlight/true#M7253
dw
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi dw
yes, this will works and it is a possible solution but it will be necessary to specify for each type of variable (neardata, fardata,nearbss etc) the ram location. There should be a method using "pragma data_core_association " and it works but it also change the location from dsram to psram (at least using the ADS linker file)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
#pragma data_core_association private0
uint32 bar0; // -> bar located into psram0
#pragma data_core_association restore
#pragma data_core_association private1
uint32 bar1; // -> bar located into psram1
#pragma data_core_association restore
#pragma data_core_association private2
uint32 bar2; // -> bar located into psram2
#pragma data_core_association restore
__private0 uint32 bar0;
__private1 uint32 bar1;
__private2 uint32 bar2;
Hi FD,
I have used pragma data_core_association as above code showed, and found PSRAM0/1/2 is allocated from local PSPR memory (start address 0xc0000000). I will report to internal team for investigate.
Thanks!
dw
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
yes, I expect it will be mapped on DSram
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Did you get some feedback?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi FD,
I have asked for internal team and perhaps this is needed to ask compiler tech support, please notice that the Tasking free toolchain's support is limited. However you could use the workaround first.
Besides, there is a PSPR code sample for your reference:
//_____________________________Locate test for CPU0 related pspr code_________________________________
#if defined(__TASKING__)
#pragma section code "psram_text_cpu0"
#elif defined(__GNUC__)
#pragma section ".psram_text_cpu0" axw
#elif defined(__DCC__)
#pragma section CODE ".psram_text_cpu0" standard RXW
#elif defined(__ghs__)
#pragma ghs section text=".psram_text_cpu0"
#endif
uint32 Locate_PsprCode_fc0(void)
{
return retData0;
}
#if defined(__GNUC__)
#pragma section
#endif