Aurix 2G User Manual Par1 Revison 1.4 Chapter 11 and Chapter 12

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
User9635
Level 4
Level 4
50 replies posted 50 questions asked 25 replies posted
Hello Support,

Aurix 2G User Manual Par1 Revison 1.4 Chapter 11 [PMS] and Chapter 12 [PMSLE] are present.
Can you please tell me what are the top level differences between these two chapters from overview perspective?
Also, are both the chapters applicable for TC387 device?
Best Regards
0 Likes
2 Replies
NeMa_4793301
Level 6
Level 6
10 likes received 10 solutions authored 5 solutions authored
Don't forget that the variant-specific appendix is part of the documentation:
TC38x_appx_um_v1.4.pdf
12 Power Management System for Low-End (PMSLE)
This device doesn’t contain a PMSLE module.
0 Likes
cwunder
Employee
Employee
100 solutions authored 5 likes given 50 likes received
If the pinout of the device has the pins VCAP0 and VCAP1 then you would refer to the PMSLE as this is a low-end device.

For the TC387 only Chapter 11 (PMS) pertains.
0 Likes