Aurix 2G TC3xx LBIST execution and PLL configuration sequence

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
User9635
Level 4
Level 4
50 replies posted 50 questions asked 25 replies posted
Hello Support,
In Aurix 2G TC3xx [TC387] devices, LBIST can be run when the CPU is put into 300MHz PLL Clock mode instead of default Back-up clock?
If no, then please point me to the User Manual Section/Page number where it is mentioned that should not be done at all.
I am assuming before LBIST execution one can configure PLL to 300MHz and switch the CPU clock without any adverse effect.
Please confirm.
Best Regards
0 Likes
2 Replies
cwunder
Employee
Employee
5 likes given 50 likes received 50 solutions authored
The user's manual clearly states the LBIST clock is supplied from the backup clock and must be scaled down for a stable LBIST execution. See the SCU chapter 9-50. Review the LBISTCTRL1.LBISTFREQU settings.
0 Likes
NeMa_4793301
Level 6
Level 6
10 likes received 10 solutions authored 5 solutions authored
Running the LBIST after PLL initialization will also result in various SMU alarms. Follow the startup sequence application note to avoid headaches.
0 Likes