Aurix 2G MCMCAN Dedicated Tx Buffer and IR Register Bit 9 [TC bit]

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
User9635
Level 4
Level 4
50 replies posted 50 questions asked 25 replies posted
Hello Support,

For Standard ID CAN Frame Transmission using Dedicated Tx Buffer from Message RAM area, I am able to see the message on the CAN bus correctly.
But for every transmission, I was expecting IR Register Bit 9 [TC bit] to be SET because the transmission was successful.
I don't see TC bit of IR register is not being SET at all.
I am using Polling Mode of CAN Transmission.
Can you please confirm whether TC bit of IR register is supposed to SET or not under the above mentioned condition?
Best regards
0 Likes
1 Reply
User9635
Level 4
Level 4
50 replies posted 50 questions asked 25 replies posted
Hello Support,
Found it.
TXBTIE Register corresponding bit of Dedicated Tx Buffer has to be enabled for TC bit of IR register to set.
Best Regards
0 Likes