Mar 19, 2020
03:40 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Mar 19, 2020
03:40 PM
Hello Support,
For Standard ID CAN Frame Transmission using Dedicated Tx Buffer from Message RAM area, I am able to see the message on the CAN bus correctly.
But for every transmission, I was expecting IR Register Bit 9 [TC bit] to be SET because the transmission was successful.
I don't see TC bit of IR register is not being SET at all.
I am using Polling Mode of CAN Transmission.
Can you please confirm whether TC bit of IR register is supposed to SET or not under the above mentioned condition?
Best regards
For Standard ID CAN Frame Transmission using Dedicated Tx Buffer from Message RAM area, I am able to see the message on the CAN bus correctly.
But for every transmission, I was expecting IR Register Bit 9 [TC bit] to be SET because the transmission was successful.
I don't see TC bit of IR register is not being SET at all.
I am using Polling Mode of CAN Transmission.
Can you please confirm whether TC bit of IR register is supposed to SET or not under the above mentioned condition?
Best regards
- Tags:
- IFX
1 Reply
Mar 19, 2020
06:16 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Mar 19, 2020
06:16 PM
Hello Support,
Found it.
TXBTIE Register corresponding bit of Dedicated Tx Buffer has to be enabled for TC bit of IR register to set.
Best Regards
Found it.
TXBTIE Register corresponding bit of Dedicated Tx Buffer has to be enabled for TC bit of IR register to set.
Best Regards