- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I am new with programming and with AURIX™ TC3x7 and TC3x4 Evaluation Kits and I have some questions:
1- I found that all the GPIO have an internal pull-up resistor (please check the screenshot attached). My question is whether it is connected to 3V3 or 5V? and if I need for example need to control a push button that requires 24VDC, how can I connect it?
2- How to configure a GPIO as tristate or pull-up with software?
3- The TC3x7 and TC3x4 Evaluation Kits contain an acoustic beeper. I would like to know if any connection should be done by hardware and how to configure it by software.
4- For the kits that contain a TFT(Touch screen), is it possible to disactivate the touch screen option and use it like a display to see only messages ?
5- I need to connect a 24VDC led to the kit, VCC_IN can power the LED, but to monitor the led (ON/OFF), does it require to add a transistor or a mosfet?
6- To wire leds and buttons to an Evaluation Board using a breadBord seems easy, but how to do it if the system should be used in an industrial environment without designing a PCB?
Looking for your advices and thanks in advance.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Dear hassna,
For, 2/3/4, you could download the source code of Application_Kit_TC397B_V2.0.0, where you will see the code example to initialize BEEP/TOUCH/TFT etc. You can disable TOUCH with TFT enabled. You can also use BEEP as the demo code showed. The entry function is as below:
#if CPU_WHICH_SERVICE_BEEPER == 0
/* initialize Acoustic Transducer */
beeper_init();
#endif
for 5), yes, as VCC_IN is only for power, the MCU needs a GPIO to get status of LED which can be a control pin for that LED.
The source code is downloaded from
dw
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Dear hassna,
For, 2/3/4, you could download the source code of Application_Kit_TC397B_V2.0.0, where you will see the code example to initialize BEEP/TOUCH/TFT etc. You can disable TOUCH with TFT enabled. You can also use BEEP as the demo code showed. The entry function is as below:
#if CPU_WHICH_SERVICE_BEEPER == 0
/* initialize Acoustic Transducer */
beeper_init();
#endif
for 5), yes, as VCC_IN is only for power, the MCU needs a GPIO to get status of LED which can be a control pin for that LED.
The source code is downloaded from
dw
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thank you for the time considered to reply my questions.
Kind regards.