Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

User18000
Level 1
Level 1
Hello!

I'm trying to enter standby mode on TC23x controller and to wake it up by PINA signal, but it doesn't work...
Here is my code:


uint16 safetyWdtPw = IfxScuWdt_getSafetyWatchdogPassword();
IfxScuWdt_clearSafetyEndinit(safetyWdtPw);

uint16 cpuWdtPw = IfxScuWdt_getCpuWatchdogPassword();
IfxScuWdt_clearCpuEndinit(cpuWdtPw);

CopyStandbyRedundancyData();
EnterStandbyMode();



__attribute__((section(".standby_code")))
void EnterStandbyMode(void) {
FLASH0_FCON.B.SLEEP = 1;

while(0 == FLASH0_FSR.B.SLM) {
}

MODULE_SCU.PMSWCR1.B.IRADIS = 0;
MODULE_SCU.PMSWCR0.B.STBYRAMSEL = 0x1;

MODULE_SCU.PMSWCR0.B.PINAEDCON = 0x3;
MODULE_SCU.PMSWCR0.B.PINADFEN = 0x1;

MODULE_SCU.PMSWCR0.B.ESR0TRIST = 1;

MODULE_SCU.PMSWCR0.B.PINAWKEN = 0x1;

MODULE_SCU.PMSWCR1.B.STBYEVEN = 1;
MODULE_SCU.PMSWCR1.B.STBYEV = 0x0;

MODULE_SCU.PMCSR[0].B.REQSLP = 0x3;
}



void CopyStandbyRedundancyData(void){
uint32_t *src = (uint32_t *)0xD0002000;
volatile uint32_t data;

uint32_t i = 0;

for (i = 0; i < 16; i++)
{
data = *src;
if ((0 == data) || (0xFFFFFFFF == data))
{
src++;
}
else
{
*src = *(uint32_t *) (data);
src++;
}
}

__isync();
__dsync();
}


.standby_code is PMI_PSPR (Scratch-Pad RAM (PSPR)) section.

Does anyone have an experience with low-power modes on Aurix MCUs?

I'll be very happy to get any suggestions...

Thanks in advance!!!
0 Likes
1 Reply
cwunder
Employee
Employee
50 solutions authored 250 sign-ins 25 likes received
I would suggest that the Safety EINIT is closed before you write to the PMCSR0 register and only use the CPU EINIT to write to the PMCSR0 register to enter standby mode. Only after CPU ENDINIT bit is set back after REQSLP is written would the REQSLP take effect.
0 Likes