Jul 30, 2021
03:54 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jul 30, 2021
03:54 AM
Hello,
I would like to use TC3XX for a SIL2 (IEC 61508) I/O module - non AUTOSAR. I have found the below SW and tools. But I have some questions:
Compiler: HighTec or Tasking. Is the compiler qualification toolkit required for SIL2?
Self test: The AURIX MCUs have LBIST, MBIST and lockstep cores etc. Is the SafeTPack library really required for SIL2? As I know,
built in HW safety features can be used at startup only as they are destructive. For cyclic tests during runtime, is a SW based self test required(e.g: MARCH test for SRAM)?
Debugger: Is the MiniWiggler can be used within HighTec and Tasking IDE?
RTOS: SafeRTOS or PXROS. Which one do you recommend?
Thanks.
I would like to use TC3XX for a SIL2 (IEC 61508) I/O module - non AUTOSAR. I have found the below SW and tools. But I have some questions:
Compiler: HighTec or Tasking. Is the compiler qualification toolkit required for SIL2?
Self test: The AURIX MCUs have LBIST, MBIST and lockstep cores etc. Is the SafeTPack library really required for SIL2? As I know,
built in HW safety features can be used at startup only as they are destructive. For cyclic tests during runtime, is a SW based self test required(e.g: MARCH test for SRAM)?
Debugger: Is the MiniWiggler can be used within HighTec and Tasking IDE?
RTOS: SafeRTOS or PXROS. Which one do you recommend?
Thanks.
Solved! Go to Solution.
- Tags:
- IFX
1 Solution
Aug 20, 2021
10:39 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Aug 20, 2021
10:39 AM
SafeTPack implements many of the external safety mechanisms listed in the Safety Manual (ESM[SW]). Many customers either develop those on their own, or choose not to implement them.
4 Replies
Aug 03, 2021
11:26 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Aug 03, 2021
11:26 PM
Up! Any reply?
Aug 09, 2021
10:17 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Aug 09, 2021
10:17 AM
Infineon just makes the chip: please check with our respective partners for those questions.
Many of the built-in hardware safety mechanisms are continuous. For RAM in particular, consider performing an MBIST at startup., Then just rely on the built-in ECC mechanisms to detect any errors that might occur during runtime. Refer to the Safety Manual for more information.
Many of the built-in hardware safety mechanisms are continuous. For RAM in particular, consider performing an MBIST at startup., Then just rely on the built-in ECC mechanisms to detect any errors that might occur during runtime. Refer to the Safety Manual for more information.
Aug 14, 2021
12:38 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Aug 14, 2021
12:38 AM
UC_wrangler wrote:
Infineon just makes the chip: please check with our respective partners for those questions.
Many of the built-in hardware safety mechanisms are continuous. For RAM in particular, consider performing an MBIST at startup., Then just rely on the built-in ECC mechanisms to detect any errors that might occur during runtime. Refer to the Safety Manual for more information.
Hello,
Thanks for the reply. But I think it's wrong to regard Infineon as only chip manufacturer. It also produces software tools and libraries (Dave, MCAL, iLLd etc). For XMC series it provides comprehensive set of solutions (compiler, debugger, libraries) but for AURIX even the technical support is provided via third parties. This is different from what its competitors offer; that makes it difficult to work with it particularly for SMEs.
The cost to start a new project from scratch is > 100k€ (tools + safety library) which may not be affordable for most SMEs.
For the question regarding safety library, it is needed to fulfill the requirements of the safety manual therefore the MCU itself can not be considered as a safety product without those SW checks. Then why is it provided via third party? It is a must for all applications which make use of AURIX.
Aug 20, 2021
10:39 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Aug 20, 2021
10:39 AM
SafeTPack implements many of the external safety mechanisms listed in the Safety Manual (ESM[SW]). Many customers either develop those on their own, or choose not to implement them.