Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

User22683
Level 1
Level 1
First reply posted First question asked
Some software functionality that is safety-critical should be executed by a lock-stepped processor in a TC27x microcontroller.

  • In the TC27x, there are two processors with checker cores, TC1.6P and TC1.6.E. I am wondering, what would be the procs/cons of choosing either of the two for such executions?
  • During start-up after a cold-reset, if only CPU0's lock-stepped mode is enabled, does this interfere with the initialization sequence shown in the attachment (copied from ap32201_TC2xx_StartupAndInitialization.pdf) ?
  • During start-up after a cold-reset, if only CPU1's lock-stepped mode is enabled, does this interfere with the initialization sequence shown in the attachment(copied from ap32201_TC2xx_StartupAndInitialization.pdf) ?
  • During start-up after a cold-reset, if both CPU0 and CPU1's lock-stepped modes are enabled, how might the initialization sequence look like?
0 Likes
1 Solution
NeMa_4793301
Level 6
Level 6
10 likes received 10 solutions authored 5 solutions authored
#1: TC1.6P is a performance core, offering a 25-30% speed improvement due to a 6-stage pipeline (vs. 4 for the TC1.6E efficiency core). The performance core does consume more current.
#2-4: Lockstep has no impact on performance or the initialization sequence.

View solution in original post

0 Likes
2 Replies
NeMa_4793301
Level 6
Level 6
10 likes received 10 solutions authored 5 solutions authored
#1: TC1.6P is a performance core, offering a 25-30% speed improvement due to a 6-stage pipeline (vs. 4 for the TC1.6E efficiency core). The performance core does consume more current.
#2-4: Lockstep has no impact on performance or the initialization sequence.
0 Likes
User22683
Level 1
Level 1
First reply posted First question asked
Thanks for your helpful feedback
0 Likes
This widget could not be displayed.