AURIX Ethernet bandwidth measurement

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Sakthivel
Level 3
Level 3
50 sign-ins 10 questions asked First like received

Hi team,

We had designed custom AURIX TC39x board. We have to find the bandwidth of AURIX ethernet.

We tried the following to measure the bandwidth:

1. Run TCP Echo server on AURIX side.

2. External peer device is accessing the server as client using Iperf.

3. Could able to connect to the running server using Iperf but Bandwidth is not properly determined.

Other method we tried:

1. Run HTTP server on AURIX side.

2. External peer device is accessing the server as client using Iperf.

3. Could able to connect to the running server using Iperf but Bandwidth is not properly determined.

Note: Both the servers are running fine, external peer device could ping the server also.

What are the tools and procedure to be followed to test the bandwidth of AURIX ethernet?? Any recommended tools?

We are planning to connect the AURIX to an external server, how to configure AURIX to be as client and connect to external TCP server, such that we can measure the AURIX ethernet bandwidth.

We want Infineon's help to test the bandwidth of AURIX ethernet. We are having NDA.

Help is most appreciated.

Regards,

Sakthivel. 

0 Likes
0 Replies