Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

ivnn
Level 1
Level 1
10 sign-ins First reply posted First like given

Hi, could anyone advice how to trigger ALM9[15] Short to Low/High Alarm by editing some registers?

0 Likes
1 Solution
µC_Wrangler
Employee
Employee
100 sign-ins 25 likes received 25 solutions authored

The CPU alarm reaction is in SMU_AG9CF0.CF15, SMU_AG9CF1.CF15, and SMU_AG9CF2.CF15 - what's in those registers?  For example, to have ALM9[15] cause an NMI, you'd configure AGiCFj per Table 528 on page 1302 of AURIXTC3XX_um_part1_v2.0.pdf:

SMU_NMI = 5 = 101b

SMU_AG9CF0.CF15 = 1

SMU_AG9CF1.CF15 = 0

SMU_AG9CF2.CF15 = 1

Also make sure SCU_TRAPDIS0.CPU0SMUT=0 (the default is 1=trap disabled).  Possibly other CPUxSMUT and SCU_TRAPDIS1.CPUxSMUT, depending on how many CPUs you want to receive the trap.

View solution in original post

0 Likes
5 Replies
µC_Wrangler
Employee
Employee
100 sign-ins 25 likes received 25 solutions authored

Hi ivnn.  Our experts warned me not to try doing that 😉

When customers want to verify their SMU configuration, my advice is usually to stay away from the fault injection path, because:

1) Some of those are extraordinarily difficult!

2) Some safety mechanisms have no fault injection mechanism, because Infineon didn't want to add the risk of accidental activation of a fault injection mechanism.

Another way of verifying the SMU configuration is to leave the SMU in START state, and then you can simply write to the alarm registers (e.g., SMU_ALM4):

In the START state software has the possibility to “emulate” the occurrence of input alarm events by writing at an
AG<x> address.

hi🤘, thanks for the quick answer!

could you pls hint the right address name to write for example for ALM9[15] 

and do we need to unlock something before write?

0 Likes
µC_Wrangler
Employee
Employee
100 sign-ins 25 likes received 25 solutions authored

Hi ivnn.  When the SMU is in start state (SMU_DBG.SSM=0), you can write to SMU_AG0...SMU_AG11.  You can see that SMU_AGi registers are Safety Endinit protected in Table 537 - Register Overview - SMU on page 1324 of AURIXTC3XX_um_part1_v2.0.pdf.

Hi, the idea was add a breakpoint in trap_handler and after ALx editing reach it

Steps:
in state SMU_DBG.SSM=0
disable ENDINIT by CBS_OCNTRL 0x000000C0 
and after the modification for example SMU_AG10  bit SF16  to 0x01 press RUN and nothing happened
Expectation was it'll stop on breakpoint but its keeps in RUN

Any ideas? maybe something else should be configured ?
Thanks

0 Likes
µC_Wrangler
Employee
Employee
100 sign-ins 25 likes received 25 solutions authored

The CPU alarm reaction is in SMU_AG9CF0.CF15, SMU_AG9CF1.CF15, and SMU_AG9CF2.CF15 - what's in those registers?  For example, to have ALM9[15] cause an NMI, you'd configure AGiCFj per Table 528 on page 1302 of AURIXTC3XX_um_part1_v2.0.pdf:

SMU_NMI = 5 = 101b

SMU_AG9CF0.CF15 = 1

SMU_AG9CF1.CF15 = 0

SMU_AG9CF2.CF15 = 1

Also make sure SCU_TRAPDIS0.CPU0SMUT=0 (the default is 1=trap disabled).  Possibly other CPUxSMUT and SCU_TRAPDIS1.CPUxSMUT, depending on how many CPUs you want to receive the trap.

0 Likes
This widget could not be displayed.