Regarding the ADS Tasking linker file, change the defined variable from the original PFLASH to the DFLASH location. Assuming I define a variable in the C code, if I don't specify a location, it will be stored in the PFLASH position by default. This is not a problem, then if I assume that I initialize and define a variable in C code, the initial specification should be at the DFLASH 0xAF00 0000 position, taking LED example code_tc297 as an example, How do I modify the Tasking Linker file?

 

smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/ADS-Tasking-linker-file/td-p/653903

0 Likes
1 Solution
Translation_Bot
Community Manager
Community Manager
Community Manager

Hi DevinHuang,

Let's fix that under this post:

https://community.infineon.com/t5/AURIX/%E9% 97 %9C% E6 %96% BCAURIX-TC297- %E6% 8C %87% E5 %AE% 9A ...

 

smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/ADS-Tasking-linker-file/m-p/654753

View solution in original post

0 Likes
1 Reply
Translation_Bot
Community Manager
Community Manager
Community Manager

Hi DevinHuang,

Let's fix that under this post:

https://community.infineon.com/t5/AURIX/%E9% 97 %9C% E6 %96% BCAURIX-TC297- %E6% 8C %87% E5 %AE% 9A ...

 

smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/ADS-Tasking-linker-file/m-p/654753

0 Likes