Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
czarlz
Level 1
Level 1
First question asked Welcome!

Does anybody have any experience in using exactly the same pin as an ADC input and a communication GPIO (out), as two alternating functions? Would it be possible to set? If so, can the GPIO drive the small capacitor that is typically needed for an SAR ADC? The communication speed can be slow (9600 or so).

Many thanks!

0 Likes
1 Reply
cwunder
Employee
Employee
100 solutions authored 5 likes given 50 likes received

If the ADC input is also on a pin that has a digital GPIO (like P0 or P33 for TC3x) then yes you can read it both via the Px_IN or with an analog conversion. When you have the pin configured as a digital output the analog reading is limited to where the output driver voltage is. 

0 Likes