A1H and A2G, Triboard is not recognized to connect via memtool on windows 10 system?

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
User17615
Level 2
Level 2
First like received
Hi all,

Triboard is not recognized to connect via memtool on windows 10 system?

Best regards,
Tita

#8042000 21402
0 Likes
1 Reply
User13836
Level 6
Level 6
50 likes received 50 solutions authored 100 sign-ins
Hello Tita,

did you install the DAS drivers? They are available at:

www.infineon.com/das

If they are installed you can use the DAS device scanner to determine if the UDAS server is running. You can also start this server manually using the DAS Device Scanner menu. This tools are included in the DAS64 program group for the 64 bit version of the DAS drivers (for 64 bit Windows) or the DAS program group for the 32 bit version (for 32 bit Windows).

When the UDAS driver is running and it does not detect the TriBoard connected you can consider to use an alternate USB cable or an alternate USB port on your PC. Or even try an alternate PC to determine if the problem you face is a PC local one.

Best regards,
Ulrich Kloidt

TASKING tools support
0 Likes