Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
explorer357
Level 1
Level 1
First reply posted First question asked Welcome!

I use  TC3XX mcal code, when I compiler the project code. Error occurs "error: missing pragma section end for data section 'Config.Cpu0.32bit' ",    it appear in the picture  . How can I solve it?

Screenshot_2024-02-06-11-20-00-694_cn.com.changan.ichangan.jpg

0 Likes
3 Replies
Jeremy_Z
Moderator
Moderator
Moderator
1000 replies posted 250 sign-ins 100 likes received

Hi @explorer357 ,

According to the figure, it's hard to figure out, so I was wondering if you could indicate the detailed error message.
BR,
Jeremy

0 Likes
Jeremy_Z
Moderator
Moderator
Moderator
1000 replies posted 250 sign-ins 100 likes received

Hi @explorer357 ,

How're things going?

BR,

Jeremy

0 Likes
Hello,
I'm sorry to just notice this email.
Following is the situlatio.
This error occurs when I configure the SPI only by Asynchronous mode. And it seems that only Asynchronous mode is not permitted to be used without synchronous mode. When I only configure synchronous mode or both mode , it wouldn't cause an error. 
By the way, it confuses me a lot in EB configuration about SPI module. Such as
1.  SpiChannelBuffersAllowed and SpiLevelDelivered these two attributes , Is there a collaborative relationship between them?
2. If I use Asynchronous mode in SPI, how should configuration DMA mode in EB, is there any example or courses?
0 Likes