三月 23, 2023
12:33 AM
将TC234L官方提供的CAN demo的loopback模式改为使用外部引脚,并且只使用CAN0 node1来发送,无法进入发送中断,请问该如何解决呀?
如果只发送一次消息的话,CANH:3.78-2.28V,CANHL:2.36V-968mv
未配置CAN0 node1引脚时, CANH:2.85左右,CANHL :2.85V左右
已解决! 转到解答。
1 解答
六月 27, 2023
11:25 PM
Please refer to this TC234 CAN demo code: https://community.infineon.com/t5/AURIX/Not-able-to-read-receiving-CAN-message-in-MultiCANBasic-Demo....
1 回复
六月 27, 2023
11:25 PM
Please refer to this TC234 CAN demo code: https://community.infineon.com/t5/AURIX/Not-able-to-read-receiving-CAN-message-in-MultiCANBasic-Demo....