如何下载BIFACES

公告

大中华汽车电子生态圈社区并入开发者社区- 更多资讯点击此

Tip / 登入 to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
闪闪
Level 1
Level 1
5 sign-ins First question asked Welcome!
 
0 点赞
1 回复
Di_W
Moderator
Moderator
Moderator
1000 replies posted 250 solutions authored 100 likes received

Hi,

Please register myICP and get Aurix Docs access right, the below link is for BIFACES.

dw

 

How to Use BIFACES

Introduction

BIFACES is an early IDE for AURIX TC2xx/TC3xx MCU, developed as a precursor to the tool ADS (Aurix Development Studio). You can use BIFACES to open early projects and employ four types of compilers: Tasking, HighTec, GreenHills, and WindRiver.

Download

To access myICP (my Infineon collaboration platform), download the following files:

  • BIFACES_V1_0_3_Win64
  • BaseProjects_TC3xx_V1_0_1_15_0_Package

You can use the latest version of BaseProjects to replace the above file.

Unzip and Install JRE 8.0

Unzip BIFACES to the following path and install JRE 8.0 as a prerequisite:

  • C:\BaseProjects_TC3xx_V1_0_1_15_0_Package
  • C:\Tools\BifacesWin64

Open BIFACES

Open StartBifaces.bat if JRE 8.0 is properly installed, and you will see the IDE interface.

Unzip

Unzip the downloaded files to the following path, and open the below path as your project's root path:

  • C:\Aurix2G_Workspace_V1_0_1_15_0\BaseFramework_TC39B

Build using Tasking

Create a project in the following path:

  • C:\Users\{Your Name}\eclipse-workspace

Or open projects in the file system and choose the following path as your first project:

  • C:\Aurix2G_Workspace_V1_0_1_15_0\BaseFramework_TC39B

Now, modify the Config.xml file in the BaseFramework_TC39B -> 1_ToolEnv -> 0_Build -> 1_Config -> Config.xml path.

Modify the root -> architecture ->primaryToolchain to Tasking.

Di_W_0-1703339488970.png

And modify the B_TASKING_TRICORE_PATH in the BaseFramework_TC39B -> 1_ToolEnv -> 0_Build -> 1_Config -> Config_Tricore_Tasking -> Config_Tasking.mk:

Di_W_1-1703339499150.png

 

B_TASKING_TRICORE_PATH =C:\Program Files\TASKING\TriCore v6.3r1\ctc
 
Install Tasking

Install Tasking Tricore 6.3r1 or later and install the compiler's licenses.

Build

If Tasking is installed properly and the primaryToolchain and B_TASKING_TRICORE_PATH are modified correctly, you can save all and start the build.

Use Examples

Copy files from the C:\Aurix2G_Workspace_V1_0_1_15_0\_Examples_TC3xx\BlinkyLed_TC39x path to your working project path:

  •  C:\Aurix2G_Workspace_V1_0_1_15_0\BaseFramework_TC39B 

Save all and build, then download the .hex using memtool, and you can see the blinking LED on your TC39x Triboard.

0 点赞