Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

AURIX™ Development Studio Forum Discussions

Sort by:
User029
AURIX™ Development Studio
Hello ,I am trying to implement lane detection or any image processing technique on SAK-TC397XX-256F300S BD  board, So using OpenMP i can get parallel... Show More
User-6_6-
AURIX™ Development Studio
Not able to toggle P33.5 by StandBy Controller (SCR), after creating a new AURIX SCR project. Any advise? See attached SCR_Toggle_P33_5_KIT_TC375_LK.z... Show More
User21369
AURIX™ Development Studio
Hi!I've been trying to debug and .elf file in Aurix Development Studio.I use a TC38x MCU with a miniwiggler v3 and I would like to flash/debug and ext... Show More
Epistemon
AURIX™ Development Studio
Hello,I'm using ADS 1.2.2 and connecting to my proprietary target board containing TC277 with miniWiggler over DAP2. Compile and link is just fine. My... Show More
Hwanen
AURIX™ Development Studio
Hello,  I basically wondered what is the C++ Standard Container support in ADS + Tasking like?I am developing a demo application for a TC397XA where I... Show More
ismMAT
AURIX™ Development Studio
I have found what we believe to be a bug regarding OneEye.When max is set to 1023 and tick-count is set to 100 in the Dial widget with 10-bit bit fiel... Show More
nsyed
AURIX™ Development Studio
Can anyone please let me know, what is the workflow for the MCAL. I am struggling to find answers to below questions. There are too many toolchains wh... Show More
JAYLOU
AURIX™ Development Studio
When I am trying to flash .elf file on my TC212L device, I got this error, what is going on? Show More
User18735
AURIX™ Development Studio
Hi all, Do anyone use TASKING Pin Mapper for initializing the input pins for Infineon Boards TC27x or TC29x (and others) in the code.If yes, could you... Show More
User22023
AURIX™ Development Studio
Hi all,where can i find the interrupt vector table?i´m working with TC387 and the Aurix Development Studio.Thanks in advance and best regards H. Show More
Forum Information

AURIX™ Development Studio

The AURIX™ Development Studio is a free of charge Integrated Development Environment (IDE) for the TriCore™-based AURIX™ microcontroller family. It is a comprehensive development environment, including Eclipse IDE, C-Compiler, Multi-core Debugger, Infineon low-level driver (iLLD), with no time and code-size limitations that enables editing, compiling, and debugging of application code. Combined with numerous code example projects, the IDE can be used to evaluate the powerful architecture of the AURIX™ microcontroller family. It supports Microsoft Windows 10 as a host operating system (OS).