AURIX™ Development Studio Forum Discussions
text.format{('custom.tabs.no.results')}
Dear Friends,
I am bird in building software. I am using HighTec Development Platform 2.0 (free version). I want to build a few source files and header files into a library file .a
How do I do that?
Thank you for your teaching.
Show LessRegister SMU_FSP displays correct value, but wrong description in the debugger view.
.B.MODE = 2 (Bi-stable protocol) --> shall be Time switching protocol.
ADS Version 1.6.0 debugging on TC397.
Show LessHi,
Anyone know where can we get the lauterbach & greenhills plugin for Aurix Development Studio?
Hi :
我在使用ADS1.8编译一组代码的时候,编译器提示错误ctc S900: internal consistency check failed - please report
这个错误可能和MISRA检查有关。
我想请问一下在ADS哪里设置可以关闭这个检查,避免这个错误警告?
thanks
-----
Hi :
When I compile a set of code with ADS1.8, the compiler prompts the error ctc S900: Internal consistency check failed - please report
This error may be related to the MISRA check.
I would like to ask where in the ADS setting can I turn off this check and avoid this false warning?
thanks
Show Less
Hi,
I`m getting this error when I build the project.
and this is the location where error happen:
I couldn`t understand why it is saying "two architectures defined with the name TC". I didn`t defined the architecture somewhere else or didn`t changed this lsl file. It is default file when I create a project.
By the way, I added lsl file here. Before this it was giving lots of unresolved external error and this is solved that problem.
how can I solve this problem?
Show Less
Hello Infineon:
before, ADS V1.5 is my building and debug tool, when I start debugging , ADS V1.5 only build the changed files.
But ADS V1.8 always re-build the whole project when start debugging.
I checked the debug configuration, there is no option to make ADS V1.8 works as V1.5.
Could you please tell me how to config ADS V1.8, then it only build the changed files?
thanks and BR
Zhou Yi
Show LessHello . Dear friend:
Could you please help me on this question?
Aurix Design Studio V1.5, TC367, Windows 10.
My questions are:
I'd like to allocate global variables and functions to specified location with #pragma as below:
#pragma section all "Calib_Data"
unsigned int speedThreshold = 100u;
#pragma section all restore
How to create RAM and ROM sections in .lsl file? It's appreciated that you give me an example project.
thanks and BR
ZhouYi
Show LessI am trying to build a project in Aurix Dev Studio Version: 1.8.0. I get the below error during linking time.
TASKING VX-toolset for AURIX Development Studio (non-commercial): control program v1.1r8 Build 22011964
Building target: demoproject.elf
ltc E821: ["C:\Infineon\AURIX-Studio-1.8.0\plugins\com.infineon.aurix.tools_1.8.0\build_system\tools\Compilers\Tasking_1.1r8\ctc\include.lsl\tc_mc_arch.lsl" 15/14] syntax error: two architectures defined with name TC
Invoking: TASKING Linker
ltc F018: Invalid LSL file, aborting...
So far I have not been able to figure out what could be the issue. I have also tried to understand how lsl files are designed but nothing seems to be resolving the issue.
Have anyone on this forum faced it and how did you resolve it? Any leads would be much appreciated!
TIA 🙂
Show LessHi there I'm attempting to run ADS on windows in a headless build mode but I'm encountering some errors. I initially used the command
"C:\Infineon\AURIX-Studio-1.8.0\Aurix-studioc.exe" -nosplash -data . -application com.tasking.managedbuilder.headlessbuild -cleanBuild all
this initially caused me some issue as I got complaints about "-perspective" being an invalid argument. I managed to solve this by making a second launcher ini with the "-perspective" argument removed. this made the command:
"C:\Infineon\AURIX-Studio-1.8.0\Aurix-studioc.exe" -nosplash -data . -application com.tasking.managedbuilder.headlessbuild -cleanBuild all --launcher.ini "C:\Infineon\AURIX-Studio-1.8.0\Aurix-studio-headless.ini"
This allows me to build the the projects (just some example project, which build perfectly fine if running in gui) and I get all the expected outputs for both projects in the workspace, with both Debug and Release built. however at the very end i then get an error pop up, informing me that there has been an error and to check the log file. I've attached the log file to this post and I was hoping someone might be able to help me figure out what's breaking
Thanks
Show LessHi,
We are compiling for Aurix Tricore TC277-D MCU using Aurix IDE version 1.8.0 (for details refer to the attached image).
When we start the debugger and disassemble the code we see a bunch of JG instructions located at various places across the code. These instructions do nothing but jump to the next instruction in sequence and they are always located right before a funtion returns.
- Are JG instructions an actual result of the compiler and are being executed by the MCU or is this some Aurix IDE viewing bug and they are not really result of the compilation?
- Why did Aurix IDE insert JG instructions? Is this deliberate or is it a bug?
- According to the TC1.6P/E instruction set JG instruction should not exist at all. What is going on?
- Concerned Tricore User