AURIX™ Development Studio Forum Discussions
1. I found the sample project for the KIT_A2G_TC377_TFT board, so, can I use the sample project ASCLIN_SHELL_UART_1_KIT_TC377_TFT for KIT_A2G_TC377_SEC_GTW board? If yes, does it affect the board by debugging this sample project to the KIT_A2G_TC377_SEC_GTW board?
2. I didn't find the example build/project for the KIT_A2G_TC377_SEC_GTW board, would someone please share the sample project for this board?
Show LessHello, I am trying to place a function into RAM (psram0) instead of flash, and I am following PAGE 3 of the Tasking LSL documentation to do so (https://resources.tasking.com/sites/default/files/uberflip_docs/file_854.pdf). I am running into this error: ltc E821: ["..\Lcf_Tasking_Tricore_Tc.lsl" 285/32] syntax error: processor name not allowed in space reference. The error occurs on this line: modify input ( space = mpe:tc0:linear ) . I am using the TC375 AURIX-Lite Development Board.
This section is where the error occurs:
derivative_tc37
{
. . .
section_setup mpe:vtc:linear
{
modify input ( space = mpe:vtc:linear )
{
select ".text.controls_pi.controls_pi";
}
}
}
We have added this section below, but are unsure whether or not it works:
/* PSRAM Code selections*/
section_layout :vtc:linear
{
/*Code Sections, selectable with patterns and user defined sections*/
group
{
/*Program Scratchpad Sections*/
group
{
. . .
group TC0_FUNCTIONS (ordered, run_addr=mem:psram0, copy )
{
select ".text.controls_pi.controls_pi";
}
}
}
}
Thank you!
Show LessHi all.
I'm trying to start working with Aurix Shield Buddy board and want to install Aurix development studio for SW development. But my company regulations require to check all licenses for new SW product. I've already checked license for main product (version 1.9.4, link), but I wasn't able to find what exact open-source and third party SW is embedded in AURIX development studio.
Can you please tell me where can I find list of all open-source license and third party software embedded in AURIX Development studio?
Show LessHello,
I am new to Tricore system and I would be glad for your help.
On TC375 microcontroller, when I locate a function to pspr using __private1 keyword and also keep a copy on Pflash using the linker file, I can see that function is in the right places checking the Memory Mapped File (copy is with [] sign in flash and function is in PSPR) , however the core1 gets stuck and returns a Trap error - Program Fetch Synchronous Error. How can I solve this?
Another thing is I can put data to PSPR, and it performs normally. Isn't PSPR for only code and I need to locate data in DSRAM?
Thanks
Show LessI found this statement in the user manual of tasking:
And I add compiler option in this step:
But it didn't work, I still find:
How to make this option useful?
Show Less
使用GTM_TIM_Capture_1_KIT_TC397_TFT的example code for TC397 demo board,Connect the TIM input port pin
P02.0 with the TOM output port pin P02.3,編譯執行結果為正常,Expressions皆可顯示PwmFreq_Hz =125、PwmDutyCycle=50 。
使用GTM_TIM_Capture_1_KIT_TC297_TFT的example code for TC297 demo board,Connect the TIM input port pin
P02.0 with the TOM output port pin P02.3,編譯執行後,但Expressions卻無法顯示正常值。
所以請問是否可協助提供GTM_TIM_Capture for TC297可正常執行的example code?
Show LessHello everyone! I am new to microcontroller programming and am having difficulty with the following implementation.
I am trying to merge the 2 examples so that the converted signal is continuously stored in memory. Despite studying the 2 linked codes and the user manual, I can't get started. Do you have a similar code or one I can start from? Thanks in advance!
Here are the 2 examples I am referring to:
Show Less
I originally wanted to debug my program, it worked for the first minute, now it's like this, I'm really crashing, I had the same problem before, and then after reinstalling ADS, it's okay, and now it's again.
Show Less